This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/OMAPL138B-EP: UART Spurious Interrupt when Transmitting

Part Number: OMAPL138B-EP

Tool/software: Linux

I'm using a CriticalLink L138F SOM in my application and have come across an interesting issue with interrupts and the UARTs on the L138.  The observed issue is that there are lots of spurious interrupts for whatever UART you are using (UART2 in my case) when transmitting characters.  This can be seen using:

cat /proc/irq/61/spurious

I can transmit characters using a simple 'echo' command or by using something like 'dd if=/dev/zero of=/dev/ttyS2 bs=8 count=8'.  Both methods create spurious interrupts.  The serial port has been set up for 115200 baud and 'raw' mode (necessary for the end application).

I'm using the Linux kernel and file system provided by CriticalLink which is based on v3.2.0.  From this I know that the serial port (tty) drivers are provided by drivers/tty/serial.8250.c.  For this version, I can see that there is a timer set up which is used to circumvent some assumed incompatibility between how the driver wants the UART peripheral to perform and how it actually performs.  More specifically the driver would like the UART to immediately raise a THRE flag the moment the interrupt flag for an empty transmitter is enabled.  The L138 doesn't do this so it uses a timer to periodically poll the interrupt register to see if there are any pending interrupts.  The issue I see with this is that you now have two sources of code trying to read the interrupt register (the timer and the real interrupt routine).  When the interrupt register is read, the interrupt flags are cleared automatically so there could be a race condition between the two and that could be a source of the spurious interrupt count increasing, because if the interrupt service routine doesn't find an interrupt to service it returns a zero, not a one (see serial8250_handle_irq in 8250.c).  I've disabled the timer and this has reduced the number of spurious interrupts seen but not completely.

Adding some debug to the 8250 driver I can output text to the console whenever a serial interrupt is raised.  Using this method, I can see that interrupts get raised for sending data (as they should) but now and again, I will get a spurious interrupt for IRQ61 (UART2) when I shouldn't.  The transmit process has completed as it should and the transmit interrupt enable has been turned off but there is still an interrupt coming from somewhere.  It doesn't happen every time but when it does, the IIR register equals 0xC1, i.e. the IPEND flag is set meaning there are no interrupts pending, yet the interrupt happened all the same.  As I have removed the timer already, there is only one point in the driver that reads the IIR register and that is in the interrupt routine.

I need some help on this because I've exhausted all other avenues.

  • Hi Simon,

    I am looking into this. I will update when I have something.

    I suppose you don't have an LCDK at your disposal to try your application on it (running the official TI Processor SDK Linux release), right?

    Best Regards,
    Yordan
  • Hi Yordan,
    I do have an LCDK but have never used it. Our application will not run on this target as we require the FPGA provided by the CriticalLink SOM (www.criticallink.com/.../) and CAN bus provided by our baseboard. I can try the LCDK and see if I get spurious interrupts by the 'cat' or 'dd' method.
  • Hi Yordan,

    I've got the LCDK working and I'm using the latest SDK from TI.  I've enabled UART1 in the device tree and this ends up enumerated as /dev/ttyS0.   I've modified the driver to add in some debug so you can see what is going on.  In the serial8250_start_tx and __stop_tx functions (8250_port.c) I print out the function name so I know when these are being called.  Also, in the serial8250_default_handle_irq function, I print out the value of iir before serial8250_handle_irq is called.

    Here's my output.  You can see that there are spurious interrupts created when sending 16 bytes to the serial port.  Every time the LSB in IIR is set, that's a spurious interrupt and there's nothing to handle.  Plus you get an interrupt AFTER __stop_tx has been called.

    root@omapl138-lcdk:~# dmesg -C
    root@omapl138-lcdk:~# stty -F /dev/ttyS0 115200 raw
    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS0 bs=16 count=1
    1+0 records in
    1+0 records out
    root@omapl138-lcdk:~# dmesg
    [  404.614981] ttyS0 - using backup timer
    [  404.615091] iir=01
    [  410.545490] ttyS0 - using backup timer
    [  410.545598] iir=01
    [  410.545894] serial8250_start_tx
    [  410.545942] __stop_tx
    [  410.545987] iir=c1
    root@omapl138-lcdk:~# cat /proc/irq/53/spurious
    count 2
    unhandled 2
    last_unhandled 110540 ms
    root@omapl138-lcdk:~#


  • Hi,

    Sorry for the delay. Just wanted to let you know that I am looking into this and will provide feedback by tomorrow morning. I've also notified the design team to elaborate in the mean time, if thy have seen such issue with the uart.

    Best Regards,
    Yordan
  • Here are my findings so far. I also enable UART1 (or serial1 in the dts files), which enumerates on ttyS1. After the board boots I run the following:

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 0

    unhandled 0

    last_unhandled 0 ms

    root@omapl138-lcdk:~# stty -F /dev/ttyS1 115200 raw                                                    

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 1

    unhandled 1

    last_unhandled 4294786856 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1                                      

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294812686 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 1

    unhandled 1

    last_unhandled 4294818286 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 1

    unhandled 1

    last_unhandled 4294823656 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294827996 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294831956 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294835416 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 1

    unhandled 1

    last_unhandled 4294840216 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 1

    unhandled 1

    last_unhandled 4294845446 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294848796 ms

    root@omapl138-lcdk:~# dd if=/dev/zero of=/dev/ttyS1 bs=16 count=1

    1+0 records in

    1+0 records out

    root@omapl138-lcdk:~# cat /proc/irq/53/spurious

    count 2

    unhandled 2

    last_unhandled 4294851496 ms

    You can see the count of spurious interrupts does not increase.

    To verify this I've looped (while 1) the sequence of commands in a script. Here is the log file & dmesg:  

    count 2
    unhandled 2
    last_unhandled 4294852826 ms
    count 2
    unhandled 2
    last_unhandled 4294852916 ms
    count 2
    unhandled 2
    last_unhandled 4294853006 ms
    count 1
    unhandled 1
    last_unhandled 4294853096 ms
    count 1
    unhandled 1
    last_unhandled 4294853186 ms
    count 2
    unhandled 2
    last_unhandled 4294853276 ms
    count 2
    unhandled 2
    last_unhandled 4294853366 ms
    count 2
    unhandled 2
    last_unhandled 4294853456 ms
    count 1
    unhandled 1
    last_unhandled 4294853546 ms
    count 2
    unhandled 2
    last_unhandled 4294853636 ms
    count 1
    unhandled 1
    last_unhandled 4294853726 ms
    count 2
    unhandled 2
    last_unhandled 4294853816 ms
    count 2
    unhandled 2
    last_unhandled 4294853906 ms
    count 2
    unhandled 2
    last_unhandled 4294853996 ms
    count 2
    unhandled 2
    last_unhandled 4294854086 ms
    count 2
    unhandled 2
    last_unhandled 4294854176 ms
    count 1
    unhandled 1
    last_unhandled 4294854266 ms
    count 1
    unhandled 1
    last_unhandled 4294854356 ms
    count 2
    unhandled 2
    last_unhandled 4294854446 ms
    count 2
    unhandled 2
    last_unhandled 4294854536 ms
    count 2
    unhandled 2
    last_unhandled 4294854626 ms
    count 1
    unhandled 1
    last_unhandled 4294854716 ms
    count 1
    unhandled 1
    last_unhandled 4294854806 ms
    count 2
    unhandled 2
    last_unhandled 4294854896 ms
    count 2
    unhandled 2
    last_unhandled 4294854986 ms
    count 2
    unhandled 2
    last_unhandled 4294855076 ms
    count 2
    unhandled 2
    last_unhandled 4294855166 ms
    count 2
    unhandled 2
    last_unhandled 4294855256 ms
    count 2
    unhandled 2
    last_unhandled 4294855366 ms
    count 2
    unhandled 2
    last_unhandled 4294855456 ms
    count 2
    unhandled 2
    last_unhandled 4294855546 ms
    count 1
    unhandled 1
    last_unhandled 4294855636 ms
    count 2
    unhandled 2
    last_unhandled 4294855726 ms
    count 1
    unhandled 1
    last_unhandled 4294855816 ms
    count 1
    unhandled 1
    last_unhandled 4294855906 ms
    count 2
    unhandled 2
    last_unhandled 4294855996 ms
    count 1
    unhandled 1
    last_unhandled 4294856086 ms
    count 1
    unhandled 1
    last_unhandled 4294856176 ms
    count 1
    unhandled 1
    last_unhandled 4294856266 ms
    count 1
    unhandled 1
    last_unhandled 4294856356 ms
    count 2
    unhandled 2
    last_unhandled 4294856456 ms
    count 2
    unhandled 2
    last_unhandled 4294856546 ms
    count 1
    unhandled 1
    last_unhandled 4294856636 ms
    count 2
    unhandled 2
    last_unhandled 4294856726 ms
    count 2
    unhandled 2
    last_unhandled 4294856816 ms
    count 2
    unhandled 2
    last_unhandled 4294856906 ms
    count 1
    unhandled 1
    last_unhandled 4294856996 ms
    count 1
    unhandled 1
    last_unhandled 4294857086 ms
    count 2
    unhandled 2
    last_unhandled 4294857176 ms
    count 1
    unhandled 1
    last_unhandled 4294857266 ms
    count 2
    unhandled 2
    last_unhandled 4294857356 ms
    count 2
    unhandled 2
    last_unhandled 4294857446 ms
    count 2
    unhandled 2
    last_unhandled 4294857536 ms
    count 2
    unhandled 2
    last_unhandled 4294857626 ms
    count 2
    unhandled 2
    last_unhandled 4294857716 ms
    count 2
    unhandled 2
    last_unhandled 4294857816 ms
    count 1
    unhandled 1
    last_unhandled 4294857906 ms
    count 2
    unhandled 2
    last_unhandled 4294857996 ms
    count 2
    unhandled 2
    last_unhandled 4294858086 ms
    count 2
    unhandled 2
    last_unhandled 4294858176 ms
    count 2
    unhandled 2
    last_unhandled 4294858266 ms
    count 2
    unhandled 2
    last_unhandled 4294858356 ms
    count 1
    unhandled 1
    last_unhandled 4294858446 ms
    count 1
    unhandled 1
    last_unhandled 4294858536 ms
    count 2
    unhandled 2
    last_unhandled 4294858626 ms
    count 2
    unhandled 2
    last_unhandled 4294858716 ms
    count 1
    unhandled 1
    last_unhandled 4294858806 ms
    count 1
    unhandled 1
    last_unhandled 4294858896 ms
    count 1
    unhandled 1
    last_unhandled 4294858986 ms
    count 1
    unhandled 1
    last_unhandled 4294859076 ms
    count 1
    unhandled 1
    last_unhandled 4294859166 ms
    count 2
    unhandled 2
    last_unhandled 4294859256 ms
    count 1
    unhandled 1
    last_unhandled 4294859346 ms
    count 1
    unhandled 1
    last_unhandled 4294859436 ms
    count 2
    unhandled 2
    last_unhandled 4294859526 ms
    count 2
    unhandled 2
    last_unhandled 4294859616 ms
    count 1
    unhandled 1
    last_unhandled 4294859706 ms
    count 1
    unhandled 1
    last_unhandled 4294859796 ms
    count 2
    unhandled 2
    last_unhandled 4294859886 ms
    count 2
    unhandled 2
    last_unhandled 4294859976 ms
    count 2
    unhandled 2
    last_unhandled 4294860066 ms
    count 2
    unhandled 2
    last_unhandled 4294860156 ms
    count 2
    unhandled 2
    last_unhandled 4294860246 ms
    count 2
    unhandled 2
    last_unhandled 4294860336 ms
    count 1
    unhandled 1
    last_unhandled 4294860426 ms
    count 2
    unhandled 2
    last_unhandled 4294860516 ms
    count 2
    unhandled 2
    last_unhandled 4294860606 ms
    count 1
    unhandled 1
    last_unhandled 4294860696 ms
    count 1
    unhandled 1
    last_unhandled 4294860786 ms
    count 2
    unhandled 2
    last_unhandled 4294860876 ms
    count 1
    unhandled 1
    last_unhandled 4294860966 ms
    count 1
    unhandled 1
    last_unhandled 4294861056 ms
    count 2
    unhandled 2
    last_unhandled 4294861146 ms
    count 1
    unhandled 1
    last_unhandled 4294861236 ms
    count 1
    unhandled 1
    last_unhandled 4294861356 ms
    count 2
    unhandled 2
    last_unhandled 4294861526 ms
    count 2
    unhandled 2
    last_unhandled 4294861616 ms
    count 2
    unhandled 2
    last_unhandled 4294861706 ms
    count 2
    unhandled 2
    last_unhandled 4294861796 ms
    count 1
    unhandled 1
    last_unhandled 4294861886 ms
    count 1
    unhandled 1
    last_unhandled 4294861976 ms
    count 2
    unhandled 2
    last_unhandled 4294862066 ms
    count 1
    unhandled 1
    last_unhandled 4294862156 ms
    count 1
    unhandled 1
    last_unhandled 4294862246 ms
    count 2
    unhandled 2
    last_unhandled 4294862336 ms
    count 2
    unhandled 2
    last_unhandled 4294862426 ms
    count 1
    unhandled 1
    last_unhandled 4294862516 ms
    count 1
    unhandled 1
    last_unhandled 4294862606 ms
    count 2
    unhandled 2
    last_unhandled 4294862696 ms
    count 2
    unhandled 2
    last_unhandled 4294862796 ms
    count 1
    unhandled 1
    last_unhandled 4294862886 ms
    count 1
    unhandled 1
    last_unhandled 4294862976 ms
    count 2
    unhandled 2
    last_unhandled 4294863066 ms
    count 1
    unhandled 1
    last_unhandled 4294863156 ms
    count 2
    unhandled 2
    last_unhandled 4294863246 ms
    count 2
    unhandled 2
    last_unhandled 4294863336 ms
    count 2
    unhandled 2
    last_unhandled 4294863426 ms
    count 2
    unhandled 2
    last_unhandled 4294863516 ms
    count 2
    unhandled 2
    last_unhandled 4294863606 ms
    count 2
    unhandled 2
    last_unhandled 4294863696 ms
    count 2
    unhandled 2
    last_unhandled 4294863786 ms
    count 2
    unhandled 2
    last_unhandled 4294863876 ms
    count 2
    unhandled 2
    last_unhandled 4294863966 ms
    count 2
    unhandled 2
    last_unhandled 4294864056 ms
    count 1
    unhandled 1
    last_unhandled 4294864146 ms
    count 2
    unhandled 2
    last_unhandled 4294864236 ms
    count 1
    unhandled 1
    last_unhandled 4294864326 ms
    count 2
    unhandled 2
    last_unhandled 4294864416 ms
    count 2
    unhandled 2
    last_unhandled 4294864506 ms
    count 2
    unhandled 2
    last_unhandled 4294864596 ms
    count 2
    unhandled 2
    last_unhandled 4294864686 ms
    count 2
    unhandled 2
    last_unhandled 4294864776 ms
    count 2
    unhandled 2
    last_unhandled 4294864866 ms
    count 2
    unhandled 2
    last_unhandled 4294864956 ms
    count 2
    unhandled 2
    last_unhandled 4294865046 ms
    count 2
    unhandled 2
    last_unhandled 4294865136 ms
    count 2
    unhandled 2
    last_unhandled 4294865226 ms
    count 2
    unhandled 2
    last_unhandled 4294865316 ms
    count 2
    unhandled 2
    last_unhandled 4294865416 ms
    count 2
    unhandled 2
    last_unhandled 4294865506 ms
    count 2
    unhandled 2
    last_unhandled 4294865596 ms
    count 1
    unhandled 1
    last_unhandled 4294865686 ms
    count 2
    unhandled 2
    last_unhandled 4294865776 ms
    count 2
    unhandled 2
    last_unhandled 4294865866 ms
    count 1
    unhandled 1
    last_unhandled 4294865956 ms
    count 2
    unhandled 2
    last_unhandled 4294866046 ms
    count 2
    unhandled 2
    last_unhandled 4294866136 ms
    count 1
    unhandled 1
    last_unhandled 4294866226 ms
    count 2
    unhandled 2
    last_unhandled 4294866316 ms
    count 2
    unhandled 2
    last_unhandled 4294866406 ms
    count 1
    unhandled 1
    last_unhandled 4294866496 ms
    count 2
    unhandled 2
    last_unhandled 4294866586 ms
    count 1
    unhandled 1
    last_unhandled 4294866676 ms
    count 1
    unhandled 1
    last_unhandled 4294866766 ms
    count 2
    unhandled 2
    last_unhandled 4294866856 ms
    count 2
    unhandled 2
    last_unhandled 4294866946 ms
    count 1
    unhandled 1
    last_unhandled 4294867036 ms
    count 2
    unhandled 2
    last_unhandled 4294867126 ms
    count 1
    unhandled 1
    last_unhandled 4294867216 ms
    count 2
    unhandled 2
    last_unhandled 4294867306 ms
    count 2
    unhandled 2
    last_unhandled 4294867396 ms
    count 2
    unhandled 2
    last_unhandled 4294867486 ms
    count 1
    unhandled 1
    last_unhandled 4294867576 ms
    count 1
    unhandled 1
    last_unhandled 4294867666 ms
    count 2
    unhandled 2
    last_unhandled 4294867756 ms
    count 2
    unhandled 2
    last_unhandled 4294867856 ms
    count 1
    unhandled 1
    last_unhandled 4294867946 ms
    count 2
    unhandled 2
    last_unhandled 4294868036 ms
    count 1
    unhandled 1
    last_unhandled 4294868126 ms
    count 2
    unhandled 2
    last_unhandled 4294868216 ms
    count 2
    unhandled 2
    last_unhandled 4294868306 ms
    count 2
    unhandled 2
    last_unhandled 4294868396 ms
    count 2
    unhandled 2
    last_unhandled 4294868486 ms
    count 2
    unhandled 2
    last_unhandled 4294868576 ms
    count 1
    unhandled 1
    last_unhandled 4294868666 ms
    count 2
    unhandled 2
    last_unhandled 4294868756 ms
    count 2
    unhandled 2
    last_unhandled 4294868846 ms
    count 1
    unhandled 1
    last_unhandled 4294868936 ms
    count 2
    unhandled 2
    last_unhandled 4294869026 ms
    count 1
    unhandled 1
    last_unhandled 4294869116 ms
    count 2
    unhandled 2
    last_unhandled 4294869206 ms
    count 2
    unhandled 2
    last_unhandled 4294869296 ms
    count 1
    unhandled 1
    last_unhandled 4294869386 ms
    count 1
    unhandled 1
    last_unhandled 4294869476 ms
    count 2
    unhandled 2
    last_unhandled 4294869566 ms
    count 2
    unhandled 2
    last_unhandled 4294869656 ms
    count 2
    unhandled 2
    last_unhandled 4294869746 ms
    count 2
    unhandled 2
    last_unhandled 4294869836 ms
    count 2
    unhandled 2
    last_unhandled 4294869926 ms
    count 2
    unhandled 2
    last_unhandled 4294870016 ms
    count 2
    unhandled 2
    last_unhandled 4294870106 ms
    count 2
    unhandled 2
    last_unhandled 4294870196 ms
    count 1
    unhandled 1
    last_unhandled 4294870286 ms
    count 2
    unhandled 2
    last_unhandled 4294870376 ms
    count 1
    unhandled 1
    last_unhandled 4294870466 ms
    count 2
    unhandled 2
    last_unhandled 4294870566 ms
    count 1
    unhandled 1
    last_unhandled 4294870656 ms
    count 2
    unhandled 2
    last_unhandled 4294870746 ms
    count 2
    unhandled 2
    last_unhandled 4294870836 ms
    count 2
    unhandled 2
    last_unhandled 4294870926 ms
    count 2
    unhandled 2
    last_unhandled 4294871016 ms
    count 2
    unhandled 2
    last_unhandled 4294871106 ms
    count 1
    unhandled 1
    last_unhandled 4294871196 ms
    count 1
    unhandled 1
    last_unhandled 4294871286 ms
    count 2
    unhandled 2
    last_unhandled 4294871386 ms
    count 2
    unhandled 2
    last_unhandled 4294871476 ms
    count 1
    unhandled 1
    last_unhandled 4294871566 ms
    count 2
    unhandled 2
    last_unhandled 4294871656 ms
    count 2
    unhandled 2
    last_unhandled 4294871746 ms
    count 2
    unhandled 2
    last_unhandled 4294871836 ms
    count 1
    unhandled 1
    last_unhandled 4294871926 ms
    count 1
    unhandled 1
    last_unhandled 4294872016 ms
    count 2
    unhandled 2
    last_unhandled 4294872106 ms
    count 1
    unhandled 1
    last_unhandled 4294872196 ms
    count 2
    unhandled 2
    last_unhandled 4294872286 ms
    count 2
    unhandled 2
    last_unhandled 4294872376 ms
    count 2
    unhandled 2
    last_unhandled 4294872466 ms
    count 2
    unhandled 2
    last_unhandled 4294872556 ms
    count 2
    unhandled 2
    last_unhandled 4294872646 ms
    count 1
    unhandled 1
    last_unhandled 4294872736 ms
    count 2
    unhandled 2
    last_unhandled 4294872836 ms
    count 2
    unhandled 2
    last_unhandled 4294872926 ms
    count 2
    unhandled 2
    last_unhandled 4294873016 ms
    count 2
    unhandled 2
    last_unhandled 4294873106 ms
    count 2
    unhandled 2
    last_unhandled 4294873196 ms
    count 2
    unhandled 2
    last_unhandled 4294873286 ms
    count 2
    unhandled 2
    last_unhandled 4294873376 ms
    count 2
    unhandled 2
    last_unhandled 4294873466 ms
    count 1
    unhandled 1
    last_unhandled 4294873556 ms
    count 2
    unhandled 2
    last_unhandled 4294873646 ms
    count 1
    unhandled 1
    last_unhandled 4294873736 ms
    count 2
    unhandled 2
    last_unhandled 4294873826 ms
    count 2
    unhandled 2
    last_unhandled 4294873916 ms
    count 1
    unhandled 1
    last_unhandled 4294874006 ms
    count 2
    unhandled 2
    last_unhandled 4294874096 ms
    count 1
    unhandled 1
    last_unhandled 4294874186 ms
    count 1
    unhandled 1
    last_unhandled 4294874276 ms
    count 1
    unhandled 1
    last_unhandled 4294874366 ms
    count 2
    unhandled 2
    last_unhandled 4294874456 ms
    count 1
    unhandled 1
    last_unhandled 4294874546 ms
    count 2
    unhandled 2
    last_unhandled 4294874636 ms
    count 2
    unhandled 2
    last_unhandled 4294874726 ms
    count 2
    unhandled 2
    last_unhandled 4294874816 ms
    count 2
    unhandled 2
    last_unhandled 4294874906 ms
    count 1
    unhandled 1
    last_unhandled 4294874996 ms
    count 1
    unhandled 1
    last_unhandled 4294875086 ms
    count 2
    unhandled 2
    last_unhandled 4294875176 ms
    count 2
    unhandled 2
    last_unhandled 4294875266 ms
    count 2
    unhandled 2
    last_unhandled 4294875356 ms
    count 1
    unhandled 1
    last_unhandled 4294875446 ms
    count 2
    unhandled 2
    last_unhandled 4294875536 ms
    count 2
    unhandled 2
    last_unhandled 4294875626 ms
    count 1
    unhandled 1
    last_unhandled 4294875716 ms
    count 2
    unhandled 2
    last_unhandled 4294875806 ms
    count 2
    unhandled 2
    last_unhandled 4294875896 ms
    count 1
    unhandled 1
    last_unhandled 4294875986 ms
    count 2
    unhandled 2
    last_unhandled 4294876076 ms
    count 1
    unhandled 1
    last_unhandled 4294876166 ms
    count 2
    unhandled 2
    last_unhandled 4294876256 ms
    count 1
    unhandled 1
    last_unhandled 4294876346 ms
    count 1
    unhandled 1
    last_unhandled 4294876436 ms
    count 1
    unhandled 1
    last_unhandled 4294876526 ms
    count 2
    unhandled 2
    last_unhandled 4294876616 ms
    count 2
    unhandled 2
    last_unhandled 4294876706 ms
    count 2
    unhandled 2
    last_unhandled 4294876796 ms
    count 2
    unhandled 2
    last_unhandled 4294876886 ms
    count 1
    unhandled 1
    last_unhandled 4294876976 ms
    count 2
    unhandled 2
    last_unhandled 4294877066 ms
    count 2
    unhandled 2
    last_unhandled 4294877156 ms
    count 2
    unhandled 2
    last_unhandled 4294877246 ms
    count 2
    unhandled 2
    last_unhandled 4294877336 ms
    count 1
    unhandled 1
    last_unhandled 4294877426 ms
    count 1
    unhandled 1
    last_unhandled 4294877516 ms
    count 2
    unhandled 2
    last_unhandled 4294877606 ms
    count 2
    unhandled 2
    last_unhandled 4294877696 ms
    count 1
    unhandled 1
    last_unhandled 4294877786 ms
    count 1
    unhandled 1
    last_unhandled 4294877886 ms
    count 2
    unhandled 2
    last_unhandled 4294877976 ms
    count 1
    unhandled 1
    last_unhandled 4294878066 ms
    count 2
    unhandled 2
    last_unhandled 4294878156 ms
    count 2
    unhandled 2
    last_unhandled 4294878246 ms
    count 2
    unhandled 2
    last_unhandled 4294878336 ms
    count 2
    unhandled 2
    last_unhandled 4294878426 ms
    count 2
    unhandled 2
    last_unhandled 4294878516 ms
    count 1
    unhandled 1
    last_unhandled 4294878606 ms
    count 2
    unhandled 2
    last_unhandled 4294878696 ms
    count 1
    unhandled 1
    last_unhandled 4294878786 ms
    count 2
    unhandled 2
    last_unhandled 4294878876 ms
    count 1
    unhandled 1
    last_unhandled 4294878966 ms
    count 2
    unhandled 2
    last_unhandled 4294879056 ms
    count 2
    unhandled 2
    last_unhandled 4294879146 ms
    count 2
    unhandled 2
    last_unhandled 4294879236 ms
    count 2
    unhandled 2
    last_unhandled 4294879326 ms
    count 1
    unhandled 1
    last_unhandled 4294879416 ms
    count 1
    unhandled 1
    last_unhandled 4294879506 ms
    count 1
    unhandled 1
    last_unhandled 4294879596 ms
    count 1
    unhandled 1
    last_unhandled 4294879686 ms
    count 1
    unhandled 1
    last_unhandled 4294879776 ms
    count 1
    unhandled 1
    last_unhandled 4294879866 ms
    count 2
    unhandled 2
    last_unhandled 4294879956 ms
    count 2
    unhandled 2
    last_unhandled 4294880046 ms
    count 1
    unhandled 1
    last_unhandled 4294880136 ms
    count 2
    unhandled 2
    last_unhandled 4294880226 ms
    count 2
    unhandled 2
    last_unhandled 4294880316 ms
    count 2
    unhandled 2
    last_unhandled 4294880406 ms
    count 2
    unhandled 2
    last_unhandled 4294880496 ms
    count 2
    unhandled 2
    last_unhandled 4294880586 ms
    count 2
    unhandled 2
    last_unhandled 4294880676 ms
    count 1
    unhandled 1
    last_unhandled 4294880766 ms
    count 2
    unhandled 2
    last_unhandled 4294880856 ms
    count 2
    unhandled 2
    last_unhandled 4294880946 ms
    count 2
    unhandled 2
    last_unhandled 4294881036 ms
    count 2
    unhandled 2
    last_unhandled 4294881126 ms
    count 2
    unhandled 2
    last_unhandled 4294881216 ms
    count 2
    unhandled 2
    last_unhandled 4294881306 ms
    count 1
    unhandled 1
    last_unhandled 4294881396 ms
    count 2
    unhandled 2
    last_unhandled 4294881486 ms
    count 2
    unhandled 2
    last_unhandled 4294881576 ms
    count 2
    unhandled 2
    last_unhandled 4294881666 ms
    count 2
    unhandled 2
    last_unhandled 4294881756 ms
    count 2
    unhandled 2
    last_unhandled 4294881846 ms
    count 2
    unhandled 2
    last_unhandled 4294881936 ms
    count 2
    unhandled 2
    last_unhandled 4294882026 ms
    count 2
    unhandled 2
    last_unhandled 4294882116 ms
    count 2
    unhandled 2
    last_unhandled 4294882206 ms
    count 1
    unhandled 1
    last_unhandled 4294882296 ms
    count 2
    unhandled 2
    last_unhandled 4294882386 ms
    count 1
    unhandled 1
    last_unhandled 4294882476 ms
    count 2
    unhandled 2
    last_unhandled 4294882566 ms
    count 2
    unhandled 2
    last_unhandled 4294882656 ms
    count 2
    unhandled 2
    last_unhandled 4294882746 ms
    count 1
    unhandled 1
    last_unhandled 4294882836 ms
    count 2
    unhandled 2
    last_unhandled 4294882936 ms
    count 2
    unhandled 2
    last_unhandled 4294883026 ms
    count 2
    unhandled 2
    last_unhandled 4294883116 ms
    count 1
    unhandled 1
    last_unhandled 4294883206 ms
    count 2
    unhandled 2
    last_unhandled 4294883296 ms
    count 2
    unhandled 2
    last_unhandled 4294883386 ms
    count 1
    unhandled 1
    last_unhandled 4294883476 ms
    count 2
    unhandled 2
    last_unhandled 4294883566 ms
    count 2
    unhandled 2
    last_unhandled 4294883656 ms
    count 1
    unhandled 1
    last_unhandled 4294883746 ms
    count 1
    unhandled 1
    last_unhandled 4294883836 ms
    count 2
    unhandled 2
    last_unhandled 4294883926 ms
    count 2
    unhandled 2
    last_unhandled 4294884016 ms
    count 2
    unhandled 2
    last_unhandled 4294884106 ms
    count 2
    unhandled 2
    last_unhandled 4294884196 ms
    count 2
    unhandled 2
    last_unhandled 4294884286 ms
    count 1
    unhandled 1
    last_unhandled 4294884376 ms
    count 1
    unhandled 1
    last_unhandled 4294884466 ms
    count 2
    unhandled 2
    last_unhandled 4294884556 ms
    count 1
    unhandled 1
    last_unhandled 4294884646 ms
    count 2
    unhandled 2
    last_unhandled 4294884736 ms
    count 1
    unhandled 1
    last_unhandled 4294884826 ms
    count 2
    unhandled 2
    last_unhandled 4294884916 ms
    count 2
    unhandled 2
    last_unhandled 4294885006 ms
    count 2
    unhandled 2
    last_unhandled 4294885096 ms
    count 2
    unhandled 2
    last_unhandled 4294885186 ms
    count 2
    unhandled 2
    last_unhandled 4294885276 ms
    count 2
    unhandled 2
    last_unhandled 4294885366 ms
    count 2
    unhandled 2
    last_unhandled 4294885456 ms
    count 1
    unhandled 1
    last_unhandled 4294885546 ms
    count 2
    unhandled 2
    last_unhandled 4294885636 ms
    count 2
    unhandled 2
    last_unhandled 4294885726 ms
    count 1
    unhandled 1
    last_unhandled 4294885816 ms
    count 2
    unhandled 2
    last_unhandled 4294885906 ms
    count 2
    unhandled 2
    last_unhandled 4294885996 ms
    count 2
    unhandled 2
    last_unhandled 4294886086 ms
    count 2
    unhandled 2
    last_unhandled 4294886176 ms
    count 2
    unhandled 2
    last_unhandled 4294886266 ms
    count 2
    unhandled 2
    last_unhandled 4294886356 ms
    count 2
    unhandled 2
    last_unhandled 4294886446 ms
    count 2
    unhandled 2
    last_unhandled 4294886536 ms
    count 2
    unhandled 2
    last_unhandled 4294886626 ms
    count 2
    unhandled 2
    last_unhandled 4294886716 ms
    count 2
    unhandled 2
    last_unhandled 4294886806 ms
    count 2
    unhandled 2
    last_unhandled 4294886896 ms
    count 2
    unhandled 2
    last_unhandled 4294886986 ms
    count 2
    unhandled 2
    last_unhandled 4294887076 ms
    count 2
    unhandled 2
    last_unhandled 4294887166 ms
    count 2
    unhandled 2
    last_unhandled 4294887256 ms
    count 2
    unhandled 2
    last_unhandled 4294887346 ms
    count 2
    unhandled 2
    last_unhandled 4294887436 ms
    count 2
    unhandled 2
    last_unhandled 4294887526 ms
    count 1
    unhandled 1
    last_unhandled 4294887616 ms
    count 2
    unhandled 2
    last_unhandled 4294887706 ms
    count 2
    unhandled 2
    last_unhandled 4294887796 ms
    count 1
    unhandled 1
    last_unhandled 4294887886 ms
    count 2
    unhandled 2
    last_unhandled 4294887986 ms
    count 1
    unhandled 1
    last_unhandled 4294888076 ms
    count 2
    unhandled 2
    last_unhandled 4294888166 ms
    count 2
    unhandled 2
    last_unhandled 4294888256 ms
    count 1
    unhandled 1
    last_unhandled 4294888346 ms
    count 2
    unhandled 2
    last_unhandled 4294888436 ms
    count 2
    unhandled 2
    last_unhandled 4294888526 ms
    count 1
    unhandled 1
    last_unhandled 4294888616 ms
    count 2
    unhandled 2
    last_unhandled 4294888706 ms
    count 1
    unhandled 1
    last_unhandled 4294888796 ms
    count 2
    unhandled 2
    last_unhandled 4294888886 ms
    count 1
    unhandled 1
    last_unhandled 4294888976 ms
    count 2
    unhandled 2
    last_unhandled 4294889066 ms
    count 1
    unhandled 1
    last_unhandled 4294889156 ms
    count 1
    unhandled 1
    last_unhandled 4294889246 ms
    count 1
    unhandled 1
    last_unhandled 4294889336 ms
    count 2
    unhandled 2
    last_unhandled 4294889426 ms
    count 2
    unhandled 2
    last_unhandled 4294889516 ms
    count 1
    unhandled 1
    last_unhandled 4294889606 ms
    count 1
    unhandled 1
    last_unhandled 4294889696 ms
    count 2
    unhandled 2
    last_unhandled 4294889786 ms
    count 1
    unhandled 1
    last_unhandled 4294889876 ms
    count 1
    unhandled 1
    last_unhandled 4294889966 ms
    count 1
    unhandled 1
    last_unhandled 4294890056 ms
    count 1
    unhandled 1
    last_unhandled 4294890146 ms
    count 2
    unhandled 2
    last_unhandled 4294890236 ms
    count 2
    unhandled 2
    last_unhandled 4294890326 ms
    count 2
    unhandled 2
    last_unhandled 4294890416 ms
    count 1
    unhandled 1
    last_unhandled 4294890506 ms
    count 1
    unhandled 1
    last_unhandled 4294890596 ms
    count 1
    unhandled 1
    last_unhandled 4294890686 ms
    count 2
    unhandled 2
    last_unhandled 4294890776 ms
    count 1
    unhandled 1
    last_unhandled 4294890866 ms
    count 2
    unhandled 2
    last_unhandled 4294890956 ms
    count 2
    unhandled 2
    last_unhandled 4294891046 ms
    count 1
    unhandled 1
    last_unhandled 4294891136 ms
    count 2
    unhandled 2
    last_unhandled 4294891226 ms
    count 2
    unhandled 2
    last_unhandled 4294891316 ms
    count 2
    unhandled 2
    last_unhandled 4294891406 ms
    count 1
    unhandled 1
    last_unhandled 4294891496 ms
    count 2
    unhandled 2
    last_unhandled 4294891656 ms
    count 1
    unhandled 1
    last_unhandled 4294891786 ms
    count 1
    unhandled 1
    last_unhandled 4294891876 ms
    count 1
    unhandled 1
    last_unhandled 4294891966 ms
    count 2
    unhandled 2
    last_unhandled 4294892056 ms
    count 2
    unhandled 2
    last_unhandled 4294892146 ms
    count 1
    unhandled 1
    last_unhandled 4294892236 ms
    count 2
    unhandled 2
    last_unhandled 4294892326 ms
    count 2
    unhandled 2
    last_unhandled 4294892416 ms
    count 2
    unhandled 2
    last_unhandled 4294892506 ms
    count 2
    unhandled 2
    last_unhandled 4294892596 ms
    count 2
    unhandled 2
    last_unhandled 4294892686 ms
    count 2
    unhandled 2
    last_unhandled 4294892776 ms
    count 1
    unhandled 1
    last_unhandled 4294892866 ms
    count 2
    unhandled 2
    last_unhandled 4294892966 ms
    count 2
    unhandled 2
    last_unhandled 4294893056 ms
    count 1
    unhandled 1
    last_unhandled 4294893146 ms
    count 1
    unhandled 1
    last_unhandled 4294893236 ms
    count 2
    unhandled 2
    last_unhandled 4294893326 ms
    count 2
    unhandled 2
    last_unhandled 4294893416 ms
    count 2
    unhandled 2
    last_unhandled 4294893506 ms
    count 2
    unhandled 2
    last_unhandled 4294893596 ms
    count 2
    unhandled 2
    last_unhandled 4294893686 ms
    count 1
    unhandled 1
    last_unhandled 4294893776 ms
    count 2
    unhandled 2
    last_unhandled 4294893866 ms
    count 2
    unhandled 2
    last_unhandled 4294893956 ms
    count 2
    unhandled 2
    last_unhandled 4294894046 ms
    count 1
    unhandled 1
    last_unhandled 4294894136 ms
    count 2
    unhandled 2
    last_unhandled 4294894226 ms
    count 2
    unhandled 2
    last_unhandled 4294894316 ms
    count 2
    unhandled 2
    last_unhandled 4294894406 ms
    count 2
    unhandled 2
    last_unhandled 4294894496 ms
    count 1
    unhandled 1
    last_unhandled 4294894586 ms
    count 2
    unhandled 2
    last_unhandled 4294894676 ms
    count 2
    unhandled 2
    last_unhandled 4294894766 ms
    count 2
    unhandled 2
    last_unhandled 4294894856 ms
    count 2
    unhandled 2
    last_unhandled 4294894946 ms
    count 2
    unhandled 2
    last_unhandled 4294895036 ms
    count 2
    unhandled 2
    last_unhandled 4294895126 ms
    count 1
    unhandled 1
    last_unhandled 4294895216 ms
    count 2
    unhandled 2
    last_unhandled 4294895306 ms
    count 2
    unhandled 2
    last_unhandled 4294895396 ms
    count 1
    unhandled 1
    last_unhandled 4294895486 ms
    count 1
    unhandled 1
    last_unhandled 4294895576 ms
    count 2
    unhandled 2
    last_unhandled 4294895666 ms
    count 1
    unhandled 1
    last_unhandled 4294895756 ms
    count 2
    unhandled 2
    last_unhandled 4294895846 ms
    count 2
    unhandled 2
    last_unhandled 4294895936 ms
    count 1
    unhandled 1
    last_unhandled 4294896026 ms
    count 2
    unhandled 2
    last_unhandled 4294896116 ms
    count 2
    unhandled 2
    last_unhandled 4294896206 ms
    count 1
    unhandled 1
    last_unhandled 4294896296 ms
    count 1
    unhandled 1
    last_unhandled 4294896386 ms
    count 1
    unhandled 1
    last_unhandled 4294896476 ms
    count 1
    unhandled 1
    last_unhandled 4294896566 ms
    count 1
    unhandled 1
    last_unhandled 4294896656 ms
    count 1
    unhandled 1
    last_unhandled 4294896746 ms
    count 2
    unhandled 2
    last_unhandled 4294896836 ms
    count 2
    unhandled 2
    last_unhandled 4294896926 ms
    count 2
    unhandled 2
    last_unhandled 4294897016 ms
    count 2
    unhandled 2
    last_unhandled 4294897106 ms
    count 2
    unhandled 2
    last_unhandled 4294897196 ms
    count 2
    unhandled 2
    last_unhandled 4294897286 ms
    count 2
    unhandled 2
    last_unhandled 4294897376 ms
    count 1
    unhandled 1
    last_unhandled 4294897466 ms
    count 1
    unhandled 1
    last_unhandled 4294897556 ms
    count 2
    unhandled 2
    last_unhandled 4294897646 ms
    count 2
    unhandled 2
    last_unhandled 4294897736 ms
    count 2
    unhandled 2
    last_unhandled 4294897826 ms
    count 1
    unhandled 1
    last_unhandled 4294897916 ms
    count 2
    unhandled 2
    last_unhandled 4294898016 ms
    count 1
    unhandled 1
    last_unhandled 4294898106 ms
    count 2
    unhandled 2
    last_unhandled 4294898196 ms
    count 2
    unhandled 2
    last_unhandled 4294898286 ms
    count 2
    unhandled 2
    last_unhandled 4294898376 ms
    count 1
    unhandled 1
    last_unhandled 4294898466 ms
    count 2
    unhandled 2
    last_unhandled 4294898556 ms
    count 1
    unhandled 1
    last_unhandled 4294898646 ms
    count 1
    unhandled 1
    last_unhandled 4294898736 ms
    count 2
    unhandled 2
    last_unhandled 4294898826 ms
    count 2
    unhandled 2
    last_unhandled 4294898916 ms
    count 2
    unhandled 2
    last_unhandled 4294899006 ms
    count 2
    unhandled 2
    last_unhandled 4294899096 ms
    count 2
    unhandled 2
    last_unhandled 4294899186 ms
    count 2
    unhandled 2
    last_unhandled 4294899276 ms
    count 2
    unhandled 2
    last_unhandled 4294899366 ms
    count 1
    unhandled 1
    last_unhandled 4294899456 ms
    count 2
    unhandled 2
    last_unhandled 4294899546 ms
    count 1
    unhandled 1
    last_unhandled 4294899636 ms
    count 1
    unhandled 1
    last_unhandled 4294899726 ms
    count 1
    unhandled 1
    last_unhandled 4294899816 ms
    count 2
    unhandled 2
    last_unhandled 4294899906 ms
    count 2
    unhandled 2
    last_unhandled 4294899996 ms
    count 1
    unhandled 1
    last_unhandled 4294900086 ms
    count 2
    unhandled 2
    last_unhandled 4294900176 ms
    count 1
    unhandled 1
    last_unhandled 4294900266 ms
    count 2
    unhandled 2
    last_unhandled 4294900356 ms
    count 1
    unhandled 1
    last_unhandled 4294900446 ms
    count 2
    unhandled 2
    last_unhandled 4294900536 ms
    count 2
    unhandled 2
    last_unhandled 4294900626 ms
    count 1
    unhandled 1
    last_unhandled 4294900716 ms
    count 2
    unhandled 2
    last_unhandled 4294900806 ms
    count 1
    unhandled 1
    last_unhandled 4294900896 ms
    count 2
    unhandled 2
    last_unhandled 4294900986 ms
    count 2
    unhandled 2
    last_unhandled 4294901076 ms
    count 1
    unhandled 1
    last_unhandled 4294901166 ms
    count 1
    unhandled 1
    last_unhandled 4294901256 ms
    count 2
    unhandled 2
    last_unhandled 4294901346 ms
    count 1
    unhandled 1
    last_unhandled 4294901436 ms
    count 2
    unhandled 2
    last_unhandled 4294901526 ms
    count 2
    unhandled 2
    last_unhandled 4294901616 ms
    count 2
    unhandled 2
    last_unhandled 4294901706 ms
    count 2
    unhandled 2
    last_unhandled 4294901796 ms
    count 2
    unhandled 2
    last_unhandled 4294901886 ms
    count 1
    unhandled 1
    last_unhandled 4294901976 ms
    count 2
    unhandled 2
    last_unhandled 4294902066 ms
    count 2
    unhandled 2
    last_unhandled 4294902156 ms
    count 2
    unhandled 2
    last_unhandled 4294902246 ms
    count 2
    unhandled 2
    last_unhandled 4294902336 ms
    count 2
    unhandled 2
    last_unhandled 4294902426 ms
    count 2
    unhandled 2
    last_unhandled 4294902516 ms
    count 1
    unhandled 1
    last_unhandled 4294902606 ms
    count 1
    unhandled 1
    last_unhandled 4294902696 ms
    count 1
    unhandled 1
    last_unhandled 4294902786 ms
    count 2
    unhandled 2
    last_unhandled 4294902876 ms
    count 1
    unhandled 1
    last_unhandled 4294902966 ms
    count 1
    unhandled 1
    last_unhandled 4294903066 ms
    count 2
    unhandled 2
    last_unhandled 4294903156 ms
    count 2
    unhandled 2
    last_unhandled 4294903246 ms
    count 2
    unhandled 2
    last_unhandled 4294903336 ms
    count 2
    unhandled 2
    last_unhandled 4294903426 ms
    count 2
    unhandled 2
    last_unhandled 4294903516 ms
    count 2
    unhandled 2
    last_unhandled 4294903606 ms
    count 2
    unhandled 2
    last_unhandled 4294903696 ms
    count 2
    unhandled 2
    last_unhandled 4294903786 ms
    count 2
    unhandled 2
    last_unhandled 4294903876 ms
    count 1
    unhandled 1
    last_unhandled 4294903966 ms
    count 2
    unhandled 2
    last_unhandled 4294904056 ms
    count 2
    unhandled 2
    last_unhandled 4294904146 ms
    count 1
    unhandled 1
    last_unhandled 4294904236 ms
    count 2
    unhandled 2
    last_unhandled 4294904326 ms
    count 2
    unhandled 2
    last_unhandled 4294904416 ms
    count 1
    unhandled 1
    last_unhandled 4294904506 ms
    count 2
    unhandled 2
    last_unhandled 4294904596 ms
    count 2
    unhandled 2
    last_unhandled 4294904686 ms
    count 2
    unhandled 2
    last_unhandled 4294904776 ms
    count 1
    unhandled 1
    last_unhandled 4294904866 ms
    count 1
    unhandled 1
    last_unhandled 4294904956 ms
    count 2
    unhandled 2
    last_unhandled 4294905046 ms
    count 1
    unhandled 1
    last_unhandled 4294905136 ms
    count 2
    unhandled 2
    last_unhandled 4294905226 ms
    count 1
    unhandled 1
    last_unhandled 4294905316 ms
    count 2
    unhandled 2
    last_unhandled 4294905406 ms
    count 1
    unhandled 1
    last_unhandled 4294905496 ms
    count 1
    unhandled 1
    last_unhandled 4294905586 ms
    count 2
    unhandled 2
    last_unhandled 4294905676 ms
    count 2
    unhandled 2
    last_unhandled 4294905766 ms
    count 2
    unhandled 2
    last_unhandled 4294905856 ms
    count 2
    unhandled 2
    last_unhandled 4294905946 ms
    count 1
    unhandled 1
    last_unhandled 4294906036 ms
    count 2
    unhandled 2
    last_unhandled 4294906126 ms
    count 1
    unhandled 1
    last_unhandled 4294906216 ms
    count 1
    unhandled 1
    last_unhandled 4294906306 ms
    count 2
    unhandled 2
    last_unhandled 4294906396 ms
    count 2
    unhandled 2
    last_unhandled 4294906486 ms
    count 2
    unhandled 2
    last_unhandled 4294906576 ms
    count 2
    unhandled 2
    last_unhandled 4294906666 ms
    count 1
    unhandled 1
    last_unhandled 4294906756 ms
    count 2
    unhandled 2
    last_unhandled 4294906846 ms
    count 2
    unhandled 2
    last_unhandled 4294906936 ms
    count 1
    unhandled 1
    last_unhandled 4294907026 ms
    count 2
    unhandled 2
    last_unhandled 4294907116 ms
    count 1
    unhandled 1
    last_unhandled 4294907206 ms
    count 2
    unhandled 2
    last_unhandled 4294907296 ms
    count 2
    unhandled 2
    last_unhandled 4294907386 ms
    count 2
    unhandled 2
    last_unhandled 4294907476 ms
    count 2
    unhandled 2
    last_unhandled 4294907566 ms
    count 1
    unhandled 1
    last_unhandled 4294907656 ms
    count 2
    unhandled 2
    last_unhandled 4294907746 ms
    count 1
    unhandled 1
    last_unhandled 4294907836 ms
    count 2
    unhandled 2
    last_unhandled 4294907926 ms
    count 1
    unhandled 1
    last_unhandled 4294908016 ms
    count 2
    unhandled 2
    last_unhandled 4294908116 ms
    count 2
    unhandled 2
    last_unhandled 4294908206 ms
    count 2
    unhandled 2
    last_unhandled 4294908296 ms
    count 2
    unhandled 2
    last_unhandled 4294908386 ms
    count 2
    unhandled 2
    last_unhandled 4294908476 ms
    count 2
    unhandled 2
    last_unhandled 4294908566 ms
    count 2
    unhandled 2
    last_unhandled 4294908656 ms
    count 1
    unhandled 1
    last_unhandled 4294908746 ms
    count 2
    unhandled 2
    last_unhandled 4294908836 ms
    count 1
    unhandled 1
    last_unhandled 4294908926 ms
    count 1
    unhandled 1
    last_unhandled 4294909016 ms
    count 1
    unhandled 1
    last_unhandled 4294909106 ms
    count 2
    unhandled 2
    last_unhandled 4294909196 ms
    count 2
    unhandled 2
    last_unhandled 4294909286 ms
    count 2
    unhandled 2
    last_unhandled 4294909376 ms
    count 2
    unhandled 2
    last_unhandled 4294909466 ms
    count 1
    unhandled 1
    last_unhandled 4294909556 ms
    count 2
    unhandled 2
    last_unhandled 4294909646 ms
    count 1
    unhandled 1
    last_unhandled 4294909736 ms
    count 2
    unhandled 2
    last_unhandled 4294909826 ms
    count 2
    unhandled 2
    last_unhandled 4294909916 ms
    count 2
    unhandled 2
    last_unhandled 4294910006 ms
    count 2
    unhandled 2
    last_unhandled 4294910096 ms
    count 2
    unhandled 2
    last_unhandled 4294910186 ms
    count 2
    unhandled 2
    last_unhandled 4294910276 ms
    count 1
    unhandled 1
    last_unhandled 4294910366 ms
    count 1
    unhandled 1
    last_unhandled 4294910456 ms
    count 2
    unhandled 2
    last_unhandled 4294910546 ms
    count 1
    unhandled 1
    last_unhandled 4294910636 ms
    count 2
    unhandled 2
    last_unhandled 4294910726 ms
    count 2
    unhandled 2
    last_unhandled 4294910816 ms
    count 1
    unhandled 1
    last_unhandled 4294910906 ms
    count 1
    unhandled 1
    last_unhandled 4294910996 ms
    count 1
    unhandled 1
    last_unhandled 4294911086 ms
    count 1
    unhandled 1
    last_unhandled 4294911176 ms
    count 1
    unhandled 1
    last_unhandled 4294911266 ms
    count 1
    unhandled 1
    last_unhandled 4294911356 ms
    count 2
    unhandled 2
    last_unhandled 4294911446 ms
    count 2
    unhandled 2
    last_unhandled 4294911536 ms
    count 1
    unhandled 1
    last_unhandled 4294911626 ms
    count 1
    unhandled 1
    last_unhandled 4294911716 ms
    count 1
    unhandled 1
    last_unhandled 4294911806 ms
    count 2
    unhandled 2
    last_unhandled 4294911896 ms
    count 1
    unhandled 1
    last_unhandled 4294911986 ms
    count 2
    unhandled 2
    last_unhandled 4294912076 ms
    count 1
    unhandled 1
    last_unhandled 4294912166 ms
    count 2
    unhandled 2
    last_unhandled 4294912256 ms
    count 2
    unhandled 2
    last_unhandled 4294912346 ms
    count 1
    unhandled 1
    last_unhandled 4294912436 ms
    count 1
    unhandled 1
    last_unhandled 4294912526 ms
    count 1
    unhandled 1
    last_unhandled 4294912616 ms
    count 1
    unhandled 1
    last_unhandled 4294912706 ms
    count 2
    unhandled 2
    last_unhandled 4294912796 ms
    count 2
    unhandled 2
    last_unhandled 4294912886 ms
    count 2
    unhandled 2
    last_unhandled 4294912976 ms
    count 2
    unhandled 2
    last_unhandled 4294913066 ms
    count 2
    unhandled 2
    last_unhandled 4294913166 ms
    count 2
    unhandled 2
    last_unhandled 4294913256 ms
    count 2
    unhandled 2
    last_unhandled 4294913346 ms
    count 2
    unhandled 2
    last_unhandled 4294913436 ms
    count 1
    unhandled 1
    last_unhandled 4294913526 ms
    count 2
    unhandled 2
    last_unhandled 4294913616 ms
    count 2
    unhandled 2
    last_unhandled 4294913706 ms
    count 2
    unhandled 2
    last_unhandled 4294913796 ms
    count 2
    unhandled 2
    last_unhandled 4294913886 ms
    count 2
    unhandled 2
    last_unhandled 4294913976 ms
    count 2
    unhandled 2
    last_unhandled 4294914066 ms
    count 2
    unhandled 2
    last_unhandled 4294914156 ms
    count 2
    unhandled 2
    last_unhandled 4294914246 ms
    count 2
    unhandled 2
    last_unhandled 4294914336 ms
    count 2
    unhandled 2
    last_unhandled 4294914426 ms
    count 1
    unhandled 1
    last_unhandled 4294914516 ms
    count 2
    unhandled 2
    last_unhandled 4294914606 ms
    count 1
    unhandled 1
    last_unhandled 4294914696 ms
    count 1
    unhandled 1
    last_unhandled 4294914786 ms
    count 1
    unhandled 1
    last_unhandled 4294914876 ms
    count 1
    unhandled 1
    last_unhandled 4294914966 ms
    count 2
    unhandled 2
    last_unhandled 4294915056 ms
    count 2
    unhandled 2
    last_unhandled 4294915146 ms
    count 2
    unhandled 2
    last_unhandled 4294915236 ms
    

    [    0.254387] NET: Registered protocol family 1
    [    0.256030] RPC: Registered named UNIX socket transport module.
    [    0.256068] RPC: Registered udp transport module.
    [    0.256082] RPC: Registered tcp transport module.
    [    0.256095] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.261620] workingset: timestamp_bits=14 max_order=15 bucket_order=1
    [    0.293189] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
    [    0.293240] io scheduler noop registered (default)
    [    0.293264] io scheduler mq-deadline registered
    [    0.293281] io scheduler kyber registered
    [    0.295732] pinctrl-single 1c14120.pinmux: 160 pins at pa fec14120 size 80
    [    0.629048] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.641911] serial8250.1: ttyS1 at MMIO 0x1d0c000 (irq = 53, base_baud = 8250000) is a TI DA8xx/66AK2x
    [    0.645266] serial8250.2: ttyS2 at MMIO 0x1d0d000 (irq = 61, base_baud = 8250000) is a TI DA8xx/66AK2x
    [    1.053309] console [ttyS2] enabled
    [    1.064664] brd: module loaded
    [    1.068558] mdio_bus fixed-0: GPIO lookup for consumer reset
    [    1.068597] mdio_bus fixed-0: using lookup tables for GPIO lookup
    [    1.068620] mdio_bus fixed-0: lookup for GPIO reset failed
    [    1.068683] libphy: Fixed MDIO Bus: probed
    [    1.077523] mdio_bus davinci_mdio.0: GPIO lookup for consumer reset
    [    1.077563] mdio_bus davinci_mdio.0: using lookup tables for GPIO lookup
    [    1.077586] mdio_bus davinci_mdio.0: lookup for GPIO reset failed
    [    1.129405] davinci_mdio davinci_mdio.0: davinci mdio revision 1.5, bus freq 2200000
    [    1.135933] davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
    [    1.143850] libphy: davinci_mdio.0: probed
    [    1.146725] davinci_mdio davinci_mdio.0: phy[7]: device davinci_mdio.0:07, driver SMSC LAN8710/LAN8720
    [    1.156699] i2c /dev entries driver
    [    1.159659] IR NEC protocol handler initialized
    [    1.162941] IR RC5(x/sz) protocol handler initialized
    [    1.166716] IR RC6 protocol handler initialized
    [    1.170367] IR JVC protocol handler initialized
    [    1.173636] IR Sony protocol handler initialized
    [    1.176974] IR SANYO protocol handler initialized
    [    1.180699] IR Sharp protocol handler initialized
    [    1.184144] IR MCE Keyboard/mouse protocol handler initialized
    [    1.188703] IR XMP protocol handler initialized
    [    1.194262] sdhci: Secure Digital Host Controller Interface driver
    [    1.199378] sdhci: Copyright(c) Pierre Ossman
    [    1.203269] davinci_mmc da830-mmc.0: GPIO lookup for consumer cd
    [    1.203306] davinci_mmc da830-mmc.0: using device tree for GPIO lookup
    [    1.203420] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/soc@1c00000/mmc@40000[0]' - status (0)
    [    1.203467] davinci_mmc da830-mmc.0: Got CD GPIO
    [    1.206843] davinci_mmc da830-mmc.0: GPIO lookup for consumer wp
    [    1.206863] davinci_mmc da830-mmc.0: using device tree for GPIO lookup
    [    1.206905] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/soc@1c00000/mmc@40000[0]'
    [    1.206936] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/soc@1c00000/mmc@40000[0]'
    [    1.206958] davinci_mmc da830-mmc.0: using lookup tables for GPIO lookup
    [    1.206980] davinci_mmc da830-mmc.0: lookup for GPIO wp failed
    [    1.260410] davinci_mmc da830-mmc.0: Using DMA, 4-bit mode
    [    1.265229] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.287205] NET: Registered protocol family 10
    [    1.294842] Segment Routing with IPv6
    [    1.297485] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    1.305048] NET: Registered protocol family 17
    [    1.322241] mmc0: host does not support reading read-only switch, assuming write-enable
    [    1.329637] console [netcon0] enabled
    [    1.332039] netconsole: network logging started
    [    1.336427] davinci_emac davinci_emac.1: incompatible machine/device type for reading mac address
    [    1.344698] mmc0: new high speed SDHC card at address aaaa
    [    1.346279] mmcblk0: mmc0:aaaa SS32G 29.7 GiB 
    [    1.353493]  mmcblk0: p1 p2
    [    1.365106] davinci_emac davinci_emac.1: using random MAC addr: 22:f5:63:a0:b2:b9
    [    1.378582] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio-keys/user1[0]' - status (0)
    [    1.378639] gpio-36 (GPIO Key USER1): gpiod_set_debounce: missing set() or set_config() operations
    [    1.378872] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio-keys/user2[0]' - status (0)
    [    1.378916] gpio-37 (GPIO Key USER2): gpiod_set_debounce: missing set() or set_config() operations
    [    1.380127] input: gpio-keys as /devices/platform/gpio-keys/input/input0
    [    1.390028] hctosys: unable to open rtc device (rtc0)
    [    1.394353] ALSA device list:
    [    1.396049]   No soundcards found.
    [    1.450412] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    1.457444] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    1.473139] random: fast init done
    [    1.481473] devtmpfs: mounted
    [    1.484411] Freeing unused kernel memory: 236K
    [    1.487595] This architecture does not have kernel memory protection.
    [    2.119072] systemd[1]: System time before build time, advancing clock.
    [    2.320649] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
    [    2.343260] systemd[1]: Detected architecture arm.
    [    2.385265] systemd[1]: Set hostname to <omapl138-lcdk>.
    [    4.491492] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.497276] systemd[1]: Reached target Remote File Systems.
    [    4.540174] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.547248] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [    4.590170] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.596845] systemd[1]: Listening on Journal Socket (/dev/log).
    [    4.643412] systemd[1]: Created slice User and Session Slice.
    [    4.681667] systemd[1]: Listening on Journal Socket.
    [    4.721626] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
    [    4.766920] systemd[1]: Created slice System Slice.
    [    5.059640] cryptodev: loading out-of-tree module taints kernel.
    [    5.087618] cryptodev: driver 1.9 loaded.
    [    5.387132] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [    7.774805] systemd-journald[63]: Received request to flush runtime journal from PID 1
    [   28.422319] davinci-rproc davinci-rproc.0: assigned reserved memory node dsp-memory@c3000000
    [   28.571160] remoteproc remoteproc0: dsp is available
    [   28.614781] alloc_contig_range: [c6440, c6441) PFNs busy
    [   29.071245] evbug: Connected device: input0 (gpio-keys at gpio-keys/input0)
    [   29.176979] remoteproc remoteproc0: powering up dsp
    [   29.239637] remoteproc remoteproc0: Booting fw image rproc-dsp-fw, size 3985484
    [   29.602926] omap_rtc 1c23000.rtc: already running
    [   29.710413] omap_rtc 1c23000.rtc: char device (253:0)
    [   29.710935] omap_rtc 1c23000.rtc: registered as rtc0
    [   30.026246] remoteproc remoteproc0: registered virtio0 (type 7)
    [   30.159569] remoteproc remoteproc0: remote processor dsp is now up
    [   30.256224] alloc_contig_range: [c6440, c6441) PFNs busy
    [   30.339886] alloc_contig_range: [c6440, c6441) PFNs busy
    [   31.167115] SCSI subsystem initialized
    [   31.212247] davinci-wdt davinci-wdt: heartbeat 60 sec
    [   31.222050] alloc_contig_range: [c6440, c6441) PFNs busy
    [   31.737369] libata version 3.00 loaded.
    [   32.058512] usbcore: registered new interface driver usbfs
    [   32.103334] vpif vpif: vpif probe success
    [   32.106405] alloc_contig_range: [c6440, c6441) PFNs busy
    [   32.120178] ahci_da850 ahci_da850: forcing PORTS_IMPL to 0x1
    [   32.120396] ahci_da850 ahci_da850: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [   32.120442] ahci_da850 ahci_da850: flags: ncq sntf pm led clo only pmp pio slum part ccc 
    [   32.121408] alloc_contig_range: [c6440, c6457) PFNs busy
    [   32.169961] scsi host0: ahci_da850
    [   32.171226] ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
    [   32.174909] alloc_contig_range: [c6440, c6441) PFNs busy
    [   32.294630] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/soc@1c00000/i2c@22000/tlv320aic3106@18[0]'
    [   32.294719] tlv320aic3x-codec 0-0018: 0-0018 supply IOVDD not found, using dummy regulator
    [   32.295075] tlv320aic3x-codec 0-0018: 0-0018 supply DVDD not found, using dummy regulator
    [   32.295324] tlv320aic3x-codec 0-0018: 0-0018 supply AVDD not found, using dummy regulator
    [   32.295637] tlv320aic3x-codec 0-0018: 0-0018 supply DRVDD not found, using dummy regulator
    [   32.295884] tlv320aic3x-codec 0-0018: Invalid supply voltage(s) AVDD: -22, DVDD: -22
    [   32.298971] alloc_contig_range: [c6440, c6441) PFNs busy
    [   32.311316] asoc-simple-card sound: ASoC: Failed to create card debugfs directory
    [   32.314021] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound[0]'
    [   32.314068] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound[0]'
    [   32.390686] alloc_contig_range: [c6440, c6460) PFNs busy
    [   32.409166] alloc_contig_range: [c6440, c6460) PFNs busy
    [   32.415275] asoc-simple-card sound: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
    [   32.659010] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [   32.659026] [drm] No driver support for vblank timestamp query.
    [   32.704967] [drm] EDID readout failed, falling back to standard modes
    [   33.262612] tvp514x 0-005d: tvp514x 0-005d decoder driver registered !!
    [   33.263195] vpif_capture vpif_capture: registered sub device tvp514x-0
    [   33.273832] vpif_capture vpif_capture: VPIF capture driver initialized
    [   33.650098] tilcdc da8xx_lcdc.0: tilcdc_crtc_irq(0x00000160): FIFO underflow
    [   33.651224] usbcore: registered new interface driver hub
    [   33.651870] usbcore: registered new device driver usb
    [   33.711993] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
    [   33.808807] Console: switching to colour frame buffer device 100x37
    [   33.832449] ohci-da8xx: DA8XX
    [   33.833275] ohci-da8xx ohci-da8xx: USB Host Controller
    [   33.833444] ohci-da8xx ohci-da8xx: new USB bus registered, assigned bus number 1
    [   33.851659] alloc_contig_range: 4 callbacks suppressed
    [   33.851697] alloc_contig_range: [c6440, c6441) PFNs busy
    [   33.852958] ohci-da8xx ohci-da8xx: irq 59, io mem 0x01e25000
    [   33.988549] hub 1-0:1.0: USB hub found
    [   33.988860] hub 1-0:1.0: 1 port detected
    [   34.116273] usb_phy_generic usb_phy_generic.0.auto: usb_phy_generic.0.auto supply vcc not found, using dummy regulator
    [   34.153675] ata1: SATA link down (SStatus 0 SControl 300)
    [   34.912813] tilcdc da8xx_lcdc.0: fb0:  frame buffer device
    [   35.029966] [drm] Initialized tilcdc 1.0.0 20121205 for da8xx_lcdc.0 on minor 0
    [   35.131201] alloc_contig_range: [c6440, c6441) PFNs busy
    [   35.161026] alloc_contig_range: [c6440, c6441) PFNs busy
    [   35.291418] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
    [   35.296159] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
    [   35.478329] hub 2-0:1.0: USB hub found
    [   35.504041] hub 2-0:1.0: 1 port detected
    [   40.160992] davinci_mdio davinci_mdio.0: resetting idled controller
    [   40.332116] SMSC LAN8710/LAN8720 davinci_mdio.0:07: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=davinci_mdio.0:07, irq=POLL)
    [   40.468930] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [   41.068064] random: crng init done
    [   41.102217] random: 7 urandom warning(s) missed due to ratelimiting
    [   47.065050] NET: Registered protocol family 15
    [   48.627452] virtio_rpmsg_bus virtio0: rpmsg host is online
    [   48.632145] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d
    [   50.703679] Initializing XFRM netlink socket
    [   56.044732] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xcc
    [   56.181529] nand: Micron MT29F4G16ABADAH4
    [   56.184374] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
    [   56.324180] Bad block table not found for chip 0
    [   56.466242] Bad block table not found for chip 0
    [   56.534675] Scanning device for bad blocks
    [   57.736814] NET: Registered protocol family 44
    [   59.801884] Bad block table written to 0x00001ffe0000, version 0x01
    [   59.808478] Bad block table written to 0x00001ffc0000, version 0x01
    [   60.189134] 3 ofpart partitions found on MTD device davinci-nand.0
    [   60.197088] Creating 3 MTD partitions on "davinci-nand.0":
    [   60.232183] 0x000000000000-0x000000020000 : "u-boot env"
    [   60.273875] 0x000000020000-0x0000000a0000 : "u-boot"
    [   60.318368] 0x0000000a0000-0x000020000000 : "free space"
    [   60.425884] davinci_nand davinci-nand.0: controller rev. 2.5
    

    As you can see the count & unhandled does not increase and there is nothing abnormal in the dmesg, so I think you can run your system without problems regarding those two spurious irqs.

    Best Regards,
    Yordan