Dear Sirs,
with reference to the DM368 device we need to use the CE0 at 16bit, in order to boot from an external NorFlash (AEMIF Config EM_A[10:8]=101b and BOOT Config EM_A[13:11]=001b), and the CE1 at 8bit because we have an SRAM and a Nand Flash byte oriented. Does is possible to differentiate per chip select the width of the Expansion Bus? Or we have to boot at 8bit from a Nor Flash byte oriented?
Thank you for your cooperation.
Loris