Part Number: TMS320C5535
I'm developing on a TMS320C5535 using the XDS110 debugger, the C5000 chip support library, and Code Composer version: 8.3.0.00009. I'm using the C5535 for a low-power application and was surprised to find that the C5535 was using about 70 mA of current when running at 100MHz with 1.3V. When I lower the frequency to 60MHz at 1.05V, the C5535 is drawing 60mA, which is extremely high according to what the datasheet claims.
After some debugging, I have narrowed down what is making the DSP draw so much current. This is a simplified version of the code I'm running:
int main(void)
{
/////////////* Variable/Structure Initializations */////////////
/* System-level variables */
CSL_Status SYS_status;
/////////////* System Level Initializations */////////////
SYS_status = SYS_PLL_LDO_init();
SYS_status |= SYS_EBSR_init();
SYS_status |= SYS_GPIO_init();
status = SPI_init();
// hspi_ADC and spiCfg_ADC are global structs
hspi_ADC->configured = FALSE;
hspi_ADC->mode = SPI_CS_NUM_0;
hspi_ADC->opMode = SPI_POLLING_MODE;
/* Set the hardware configuration */
spiCfg_ADC.spiClkDiv = 20;
spiCfg_ADC.wLen = SPI_WORD_LENGTH_32;
spiCfg_ADC.frLen = 1;
spiCfg_ADC.wcEnable = SPI_WORD_IRQ_DISABLE;
spiCfg_ADC.fcEnable = SPI_FRAME_IRQ_DISABLE;
spiCfg_ADC.csNum = SPI_CS_NUM_0;
spiCfg_ADC.dataDelay = SPI_DATA_DLY_0;
spiCfg_ADC.csPol = SPI_CSP_ACTIVE_LOW;
spiCfg_ADC.clkPol = SPI_CLKP_LOW_AT_IDLE; // SPI MODE 1
spiCfg_ADC.clkPh = SPI_CLK_PH_RISE_EDGE;
SYS_status |= SPI_config(hspi_ADC, &spiCfg_ADC);
/////////////* Infinite Loop */////////////
while (1)
{
} // while()
} // main()
This codes causes the DSP at 100MHz to draw 70mA and 60MHz to draw 60mA, which is a crazy amount of current for a low power application.
However, I then comment out the SPI_init():
CSL_Status SYS_SPI_init(){
CSL_Status status;
//status = SPI_init();
hspi_ADS->configured = FALSE;
hspi_ADS->mode = SPI_CS_NUM_0;
hspi_ADS->opMode = SPI_POLLING_MODE;
.
.
.
With SPI_init() commented out, the current consumption is now much more reasonable:
100MHz draws about 20mA, 60Mhz draws about 13mA
Why is the SPI peripheral being such a power hog? I even changed the SPI clock frequency from 5MHz to 100kHz, but the large current draw of 70mA/60mA persists.
One of the ways I tried to get around this was to uninitialized SPI when I'm done sending data using SPI. Even after using SPI_deinit(), the current consumption of the C5535 stays at 70mA/60mA. I'm only able to reduce the current consumption if I don't call SPI_init() at all.
I'm really trying to get as close to 10mA as possible. Are there any suggestions for how I can reduce the power consumption of the SPI peripheral? Is it expected that the SPI peripheral consumes so much current?
Best,
Eddie