This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: TMS320C6748

Part Number: TMS320C6748

Dear friends,

I am using the L138/C6748 LCDK development kit on which having one External Flash and External SDRAM.

I want to do bootloading for this platform. i have downladed the C6748Starterware.exe and installed.

In starterware bootloader example code is given.In which SPI,  NAND, MMSd  methods are there.

in another bootloader example UART & SPI,  NAND, MMSd also available.

Actually I need to receive file through UART and then I have to write on FLASH. Later using the Bootloader example NANDbootcopy 

I have read from FLASH and write to the Device Internal RAM.

So I downlaoded AISgen tool and read the detailed File Conversion thing.

q1) For this how I have to write UBL (user boot loader) or any custom example is there for it?  or I have to UART_Boot_Copy() from the Bootloader?

q2) As in Starterware Bootloader example UART_boot_copy() method.

 "     int XmodemReceive(unsigned char *dest, int destz)     "

What this function will do ?Will it read from UART and write to RAM .

 

I need reference and any links for completing this task.Please help me for this.

 

 

Regards,

Ashrumochan