Other Parts Discussed in Thread: PCF8574A, THS7303, THS7353, TVP7002
Hi,
i'm trying use the new dvsdk 3_10_00_19 on Ubuntu 10.04 for my dm6467 EVM. Everything apparently worked fine until the NFS mounting of directories. Here are the outputed problems:
/***********************************/
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
eth0: attached PHY driver [ET1011C] (mii_bus:phy_addr=1:01, id=282f013)
Sending DHCP requests ..
PHY: 1:01 - Link is Up - 1000/Full
., OK
IP-Config: Got DHCP answer from 10.0.0.1, my address is 10.0.0.25
IP-Config: Complete:
device=eth0, addr=10.0.0.25, mask=255.255.255.0, gw=10.0.0.1,
host=10.0.0.25, domain=, nis-domain=(none),
bootserver=10.0.0.1, rootserver=10.0.0.1, rootpath=
Looking up port of RPC 100003/2 on 10.0.0.1
rpcbind: server 10.0.0.1 not responding, timed out
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 10.0.0.1
rpcbind: server 10.0.0.1 not responding, timed out
Root-NFS: Unable to get mountd port number from server, using default
Root-NFS: Server returned error -5 while mounting /tftpboot/10.0.0.25
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
0300 39070080 hda driver: ide-gd
0301 35158221 hda1
0302 3911827 hda2
1f00 128 mtdblock0 (driver?)
1f01 1280 mtdblock1 (driver?)
1f02 4096 mtdblock2 (driver?)
1f03 125568 mtdblock3 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Backtrace:
[<c00307d0>] (dump_backtrace+0x0/0x114) from [<c0310d7c>] (dump_stack+0x18/0x1c)
r7:00008000 r6:c5012000 r5:c0026808 r4:c0426c10
[<c0310d64>] (dump_stack+0x0/0x1c) from [<c0310dd4>] (panic+0x54/0x124)
[<c0310d80>] (panic+0x0/0x124) from [<c0008fbc>] (mount_block_root+0x1e0/0x220)
r3:00000001 r2:c5025e98 r1:c5025f60 r0:c039c58d
[<c0008ddc>] (mount_block_root+0x0/0x220) from [<c00090c0>] (mount_root+0xc4/0xfc)
r8:00000000 r7:00000000 r6:00000000 r5:00000000 r4:00200000
[<c0008ffc>] (mount_root+0x0/0xfc) from [<c0009268>] (prepare_namespace+0x170/0x1c8)
r5:c0026808 r4:c0426700
[<c00090f8>] (prepare_namespace+0x0/0x1c8) from [<c00084bc>] (kernel_init+0xe4/0x118)
r5:00000000 r4:c04264c0
[<c00083d8>] (kernel_init+0x0/0x118) from [<c0045964>] (do_exit+0x0/0x684)
r5:00000000 r4:00000000