Part Number: TMDXIDK5718
Tool/software: Linux
Hi
I'm using TI SDK 5.3.0.7
I want to set a static IP for eth0 and have the interface up and running after boot.
I added the following to /etc/network/interfaces
auto eth0
iface eth0 inet static
address 10.41.140.196
netmask 255.255.254.0
gateway 10.41.140.1
Still using DHCP
Then I read and executed
The effect that no ethernet interface is up anymore after boot except for loopback.
Regards, Chris