hi, everyone:
I'm using DM365 BETA_board to working on 720P MPEG4 decode+display, as the BETA-board have the earliest kernel and system image, which haven't the demo I want , so, I update the flash_image system, but got an problem when excute "./loadmodules_hd.sh" like:
irqk: disagrees about version of symbol struct_module
insmod: error inserting 'cmemk.ko': -1 Invalid module format
insmod: error inserting 'irqk.ko': -1 Invalid module format
edmak: disagrees about version of symbol struct_module
dm365mmap: disagrees about version of symbol struct_module
insmod: error inserting 'edmak.ko': -1 Invalid module format
insmod: error inserting 'dm365mmap.ko': -1 Invalid module format
someone knows this problem? By the way, I use TFTP to download the uImage I maked which was the newest "linux-2.6.18_pro500" and I haven't overwrite the board kernel, so, any suggest will be appreciate!