Part Number: AM5728
Other Parts Discussed in Thread: PCM1681
Tool/software: Linux
Hi,
I want to capture 8 mic data at a time so i am using McASP2 of Beagleboard X15 . I need help on these questions:-
1). how bitclk and Fsclk is configure at specific pin
2). If i want to record in minicom i am getting this error:-
arecord -f S16_LE Mcasp2_1mic.wav -c 2 -r 96000
Recording WAVE 'Mcasp2_1mic.wav' : Signed 16 bit Little Endian, Rate 96000 Hz, Stereo
[ 1463.776298] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:757: group 2, block bitmap and bg descriptor inconsistent: 10370 vs 12418 frees
[ 1463.791240] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:757: group 3, block bitmap and bg descriptor inconsistent: 7700 vs 20242 frees
3). i ahve done these configurations:-
sound2: sound2 {
compatible = "simple-audio-card";
simple-audio-card,name = "PCM1681";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&sound2_master>;
simple-audio-card,frame-master = <&sound2_master>;
simple-audio-card,bitclock-inversion;
simple-audio-card,cpu {
sound-dai = <&mcasp2>;
};
sound2_master: simple-audio-card,codec {
sound-dai = <&pcm1681>;
clocks = <&clkout2_clk>;
clock-names = "mclk";
};
};
};
&dra7_pmx_core {
mcasp2_pins: mcasp2_pins {
pinctrl-single,pins= <
/* sink must enable transmitter/receivers*/
0x2f4 (PIN_INPUT_PULLDOWN | MUX_MODE0)
0x2f8 (PIN_INPUT_PULLDOWN | MUX_MODE0)
0x304 (PIN_OUTPUT_PULLDOWN | MUX_MODE0)
0x308 (PIN_OUTPUT_PULLDOWN | MUX_MODE0)
>;
};
&mcasp2 {
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&mcasp2_pins>;
//assigned-clocks = <&mcasp2_ahclkx_mux>;
//assigned-clock-parents = <&sys_clkin2>;
status = "okay";
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
/* 16 serializers */
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
2 2 2 2
2 2 2 2
0 0 0 0
0 0 0 0
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
i have made changes in am57xx-beagleboardx-15-common.dtsi file
if any other files need to be changed please let me know as i don't know about device driver .
Thanks,
Pooja