Part Number: TDA2-17
Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hi Sir,
I am running AVB surround view case.
There are 4 AVB cameras through a 100/1000 base Ethernet switch to connect to TDA2 EVM.
My AVB camera uses 100 Mbps phy to transmit the data.
Because of this Ethernet switch limit, when connecting camera with 100 Mbps data rate,
All switch port becomes 100Mbps band width. It means if amount data rate of 4 cameras is over than 100 Mbps,
Ethernet switch can't handle it.
May you suggest which "Ethernet switch" can handle 100 Mbps camera input and output 1000Mbps at the same time?
May provide the product brand and part number.
Thank you.
Ranny.