This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/SYSBIOS: Select SYS/BIOS .cfg file by project CCS build configuration

Part Number: SYSBIOS


Tool/software: TI-RTOS

Hi,

I have a project that gets built for various CCS build configurations, let's say DEBUG1/RELEASE1/DEBUG2/RELEASE2.

DEBUG2/RELEASE2 are new and they need a new SYSBIOS .cfg file.

I need a way to specify in DEBUG1/RELEASE1 that XDCTOOLS should build only SYSBIOS1.cfg.

And of course, DEBUG2/RELEASE2 -> should build only SYSBIOS2.cfg.

Both SYSBIOS1.cfg and SYSBIOS2.cfg are in my project directory tree root.

A 2nd method would to use a common SYSBIOS.cfg for both an figure out in the .cfg itself which is the CCS build configuration but the syntax of .cfg is undocumented.

For both of these methods I can't find any documentation in the SYSBIOS manual.

Hope I get some help here.

Thanks.