Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
I want to install the recently released "PROCESSOR-SDK-LINUX-RT-AM335X 05_03_00_07" using
"Building the SDK" instructions.
During the layer configuration for this particular release (Processor SDK 05.03.00.07) and after
cloning "git://arago-project.org/git/projects/oe-layersetup.git", I haven't found the
expected config file for this SDK "configs/processor-sdk/processor-sdk-05.03.00.07-config.txt"
Should I use the the config file of the previous SDK "processor-sdk-05.02.00.10-config.txt" or
is the file "processor-sdk-05.03.00.07-config.txt" missing?
Thanks.