Part Number: AM3358
Hi!
Recently I received a request to develop a custom PCB with video loop functionality. It have to loop video or switch between videos without delay (at least lower then 100ms delay) and without blank spaces. Another request is Full HD resolution. I can use any codec I like. The board have some other things to do but only videoplayback is a field where I don't feel myself confident enough.
So long story short - is it possible to do it with AM3358 processor?
I'm asking because I'm willing to buy development board earlier to not waste my time since delivery will probably take one or two weeks to the place where I live.
Also I greatly appreciate any recommendations if there is a processor better suited for this purpose.