Tool/software: Linux
hai,
i am using winbond W25Q64FW nor flash with am5728, is it possible to flash this memory using user space application. That is, is it possible write an user space application which takes a file as input and flash this to the address mentioned by the user.
If it is possible, i want to know, if any other file like an user application(test.out) is required to be flashed into nor flash and then make it to run by using the address location of file in nor flash.
thanks & regards,
Venkat R.