This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: Enabling 10 inch LCD display, and play video

Part Number: TDA2EVM5777

Tool/software: Linux

HI,

I am connecting the 10 inch LCD/touch screen display to the TDA2xx 5777 EVM.

I have connected the flat connecting cable between the LCD and the EVM.

I am running linux on the board, which is running fine. I get the command prompt.

But i do not get any thing on the LCD display.

Is there any script to test the LCD display?

Do we need to do any thing additional to enable it.

One point observed is that the flat cable connects straight, with the black color at the end facing the top and the exposed electrodes towards the PCB. But the '1' marked on the CPU board does not match the '1" on the LCD. Is the connection correct? Since the cable is flat cannot twist it.

Also, does the vision SDK has the utilities like gstreamer to play video on the board?

Kinldy let me know

Thanks and Regards,

Archit Adwant