Part Number: AM5728
Tool/software: Linux
hi,
i am working with am5728 with spi nor flash. I flashed three binary files into NOR flash at different address locations corresponding to size of files using uboot commands(NOR flash has no file systems or partitions). Among the three applications, one is an application binary that should use the other two binary files as an input to append these two files. All i did is, just flashed the NOR flash with binaries but, I need help in knowing how these can be used and append two of the files using application binary.
I think there should a process on how to do it. Please help me with issue.
Thanks & Regards,
venkat R.