Other Parts Discussed in Thread: OMAP-L137, DA8XX
Hello
I'm using OMAP-L137 Spectrum digital EVM and all the install code from
http://processors.wiki.ti.com/index.php/Installing_the_Software_for_OMAP-L137
and
http://processors.wiki.ti.com/index.php/Setting_up_OMAP-L137_Target_File_System
under Ubuntu and VMwhare player. Seems things are installed correctly and doing a EVM terminal boot I get...
U-Boot > boot
BOOTP broadcast 1
DHCP client bound to address 192.168.1.116
TFTP from server 192.168.1.1; our IP address is 192.168.1.116
Filename 'uImage'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
############################
done
Bytes transferred = 1804692 (1b8994 hex)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.18_pro500-da830_omapl1
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1804628 Bytes = 1.7 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux........................................................................................................................ done, booting the kernel.
Linux version 2.6.18_pro500-da830_omapl137_evm-arm_v5t_le (x0029463@aspbuild11) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Thu Apr 23 17:41:16 IST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DA8XX EVM
Memory policy: ECC disabled, Data cache writethrough
DA830 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
Built 1 zonelists. Total pages: 8192
Kernel command line: console=ttyS2,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.1:/home/user/workdir/filesys,nolock mem=32M
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 28516KB available (3092K code, 632K data, 176K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 128 gpio irqs
Generic PHY: Registered new driver
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 256 (order: -2, 1024 bytes)
TCP established hash table entries: 1024 (order: 0, 4096 bytes)
TCP bind hash table entries: 512 (order: -1, 2048 bytes)
TCP: Hash tables configured (established 1024 bind 512)
TCP reno registered
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS version 1.0, (C) 1999, 2000 Axis Communications AB
JFFS2 version 2.2. (NAND) (SUMMARY) (C) 2001-2006 Red Hat, Inc.
yaffs Apr 23 2009 17:39:03 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c42000 mem 0xfec42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfed0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO map 0x1d0d000 mem 0xfed0d000 (irq = 61) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is 00:0e:99:02:f8:2e
TI DaVinci EMAC Linux version updated 4.0
i2c /dev entries driver
Creating 3 MTD partitions on "Windbond spi nand flash":
0x00000000-0x00040000 : "U-Boot"
0x00040000-0x00044000 : "U-Boot Environment"
0x00044000-0x00400000 : "Linux"
dm_spi.0: davinci SPI Controller driver at 0xc285c000 (irq = 20) use_dma=1
dm_spi.1: davinci SPI Controller driver at 0xc285e000 (irq = 56) use_dma=1
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new driver libusual
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Waiting for USB PHY clock good...
musb_hdrc: USB Host mode controller at c2860000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
usb usb2: configuration #1 chosen from 1 choice
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
rtc-da8xx rtc-da8xx.0: rtc intf: proc
rtc-da8xx rtc-da8xx.0: rtc intf: dev (254:0)
rtc-da8xx rtc-da8xx.0: rtc core: registered rtc-da8xx as rtc0
rtc-da8xx rtc-da8xx.0: TI DA8xx Real Time Clock driver.
davinci-mmc davinci-mmc.0: Supporting 8-bit mode
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.2
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DA8XX EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc-da8xx rtc-da8xx.0: setting the system clock to 2000-01-01 20:39:06 (946759146)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.1.1, my address is 192.168.1.102
IP-Config: Complete:
device=eth0, addr=192.168.1.102, mask=255.255.255.0, gw=255.255.255.255,
host=192.168.1.102, domain=example.org, nis-domain=(none),
bootserver=192.168.1.1, rootserver=192.168.1.1, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.1
Looking up port of RPC 100005/1 on 192.168.1.1
VFS: Mounted root (nfs filesystem).
Freeing init memory: 176K
Warning: unable to open an initial console.
Kernel panic - not syncing: No init found. Try passing init= option to kernel.
Can anyone tell me what this Kernel panic means and how to fix it?
Thanks Brian