This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How Can I use EDMA in DM365 SPI ?



How Can I use EDMA in DM365 SPI ?

I tyied ,but failed.

1./arch/arm/math-davinci/davinci-spi-platform.c

static struct resource dm3xx_spi_resources[] = {
 [0] = {
  .start = DM3XX_SPI0_BASE,
  .end = DM3XX_SPI0_BASE + (SZ_4K/2) - 1,
  .flags = IORESOURCE_MEM,
 },
 [1] = {
  .start = IRQ_DM3XX_SPINT0_0,
  .end = IRQ_DM3XX_SPINT0_0,
  .flags = IORESOURCE_IRQ,
 },
 [2] = {
  .start = DM365_DMA_SPI0REVT,
  .end = DM365_DMA_SPI0REVT,
  .flags = IORESOURCE_DMA | IORESOURCE_DMA_RX_CHAN,
 },
 [3] = {
  .start = DM365_DMA_SPI0XEVT,
  .end = DM365_DMA_SPI0XEVT,
  .flags = IORESOURCE_DMA | IORESOURCE_DMA_TX_CHAN,
 },
 [4] = {
  .start = EVENTQ_3,
  .end = EVENTQ_3,
  .flags = IORESOURCE_DMA | IORESOURCE_DMA_EVENT_Q,
 },

};

2. I wrote a user program to read the eeprom

#include <stdio.h>
#include <unistd.h>
#include <stdlib.h>
#include <fcntl.h>

int main(){

  int eepromfd;
  unsigned char loop;
  unsigned char data[16];

  eepromfd = open("/dev/mtd5",O_RDWR );
  if(eepromfd == -1){
    printf("cannot open mtd5\n");
    return -1;
  }

  printf("fd is %d\n",eepromfd);

  printf("No of Bytes Read = %d\n",read(eepromfd,data,16));

  for(loop=0;loop<16;loop++){
    if((loop%8)==0){
      printf("\n");
    }
    printf("%02X ",data[loop]);
  }
  printf("\n");

  close(eepromfd);

  return 0;

If I do not change dm3xx_spi_resources[] (do not use dma),I can work with the EEPROM well.

But if I change dm3xx_spi_resources[] ( use dma), I can not work with the EEPROM.

The software can not go into davinci_spi_dma_tx_callback() or davinci_spi_dma_rx_callback() in /drivers/spi/davinci_spi_master.c

What can I do to use DMA in DM365 SPI?