Hi,
I have another quesion about the MMC/SD card controller,because of the limit of SDIO spec 2.0 ,the max clock for the SDIO is 50M,
The MMC/SD card controller supports MMC (Multimedia Card) Specification v4.0,is the max clock also 50M or more?
Thanks.