Tool/software: Linux
Hi,
I have successfully build and put the image on the sd card. I can get into the root and when I tried to run app.out it keeps on running attaching to ipu1 and other processing units without showing any particular display of the demo usecases. Can anyone help me figure this thing out?
root@dra7xx-evm:/opt/vision_sdk# source ./vision_sdk_load.sh insmod: ERROR: could not insert module ./bin/memcache.ko: File exists insmod: ERROR: could not load module ./bin/cmemk.ko: No such file or directory mknod: /dev/memcache: File exists ./disableDssInterruptsOnA15.sh: line 11: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 12: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 13: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 14: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 15: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 16: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 17: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 18: COMMANDS: command not found ./disableDssInterruptsOnA15.sh: line 19: COMMANDS: command not found updated value is COMMANDS ### WARNING ###: use the following [read | write | set bit | clear bit | dump] commands at your own risk! No address check done, may generate: - bus error (invalid or not accessible <physical address>, - platform crash/hang (bad <value>). Read any OMAP memory address (register), given its <physical address> or <name> as listed in TRM. Write <value> at any OMAP memory address (register), given its <physical address> or <name> as listed in TRM. Set bit at <position> into any OMAP memory address (register), given its <physical address> or <name> as listed in TRM. Clear bit at <position> into any OMAP memory address (register), given its <physical address> or <name> as listed in TRM. Dump a range of OMAP memory addresses, from <start address> to <end address>. Note all addresses within given range must be valid and accessible. ### WARNING ###: use the following I2C [read | write] commands at your own risk! No address check done, may generate: - I2C bus error (invalid or not accessible <physical address>, - platform crash/hang (bad <value>). Read I2C register at address <addr> from I2C chip at <chip-addr> on I2C <bus>. Write <value> in I2C register at address <addr> from I2C chip at <chip-addr> on I2C <bus>. root@dra7xx-evm:/opt/vision_sdk# ./apps.out [HOST] OSA: MEM: 0: Mapped 0xa0100000 to 0xb697f000 of size 0x00100000 [HOST] OSA: MEM: 1: Mapped 0x84203000 to 0xa3d7f000 of size 0x12c00000 [HOST] OSA: MEM: 2: Mapped 0xa0200000 to 0xa3cbf000 of size 0x00040000 [HOST] OSA: MEM: 3: Mapped 0xa02c0000 to 0xa3cff000 of size 0x00080000 [HOST] OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000 [HOST] OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000 [HOST] OSA: HOST Remote Log Shared Memory @ 0xa024f140 [HOST] OSA: DSP1 Remote Log Shared Memory @ 0xa02769e0 [HOST] OSA: DSP2 Remote Log Shared Memory @ 0xa029e280 [HOST] OSA: EVE1 Remote Log Shared Memory @ 0xa02c5b20 [HOST] OSA: EVE2 Remote Log Shared Memory @ 0xa02ed3c0 [HOST] OSA: EVE3 Remote Log Shared Memory @ 0xa0314c60 [HOST] OSA: EVE4 Remote Log Shared Memory @ 0xa033c500 [HOST] OSA: IPU2 Remote Log Shared Memory @ 0xa0363da0 [HOST] [IPU1-0] 1957.479259 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1958.479289 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1959.479320 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1960.479350 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1961.479381 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1962.479411 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1963.479442 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1964.479442 s: SYSTEM: Attaching to [IPU2] ... [HOST] [HOST ] 1964.546391 s: SYSTEM: System A15 Init in progress !!! [HOST] [DSP1 ] 1957.570853 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1958.570883 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1959.570914 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1960.570944 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1961.570975 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1962.571005 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1963.571036 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1956.710852 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1957.710882 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1958.710882 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1959.710913 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1960.710943 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1961.710974 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1962.711004 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1963.711035 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1964.571066 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1964.711065 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1965.479472 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1965.571066 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1965.711096 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1966.479503 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1966.571097 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1966.711096 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1967.479533 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1967.571127 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1967.711126 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1968.479564 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1968.571158 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1968.711157 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1969.479594 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1969.571188 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1969.711187 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1970.479625 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1970.571219 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1970.711218 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1971.479655 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1971.571249 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1971.711248 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1972.479686 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1972.571280 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1972.711279 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1973.479686 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1973.571280 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1973.711309 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1974.479716 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1974.571310 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1974.711340 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1975.479747 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1975.571341 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1975.711340 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1976.479777 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1976.571371 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1976.711370 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1977.479808 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1977.571402 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1977.711401 s: SYSTEM: Attaching to [IPU2] ... [HOST] [IPU1-0] 1978.479838 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP1 ] 1978.571432 s: SYSTEM: Attaching to [IPU2] ... [HOST] [DSP2 ] 1978.711431 s: SYSTEM: Attaching to [IPU2] ...