Will redundancy protocols like DLR,MRP and HSR are implemented in PRU-ICSS(i.e. hardware level), or it should be a part of protocol stack of Ethernet/IP, Profinet ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will redundancy protocols like DLR,MRP and HSR are implemented in PRU-ICSS(i.e. hardware level), or it should be a part of protocol stack of Ethernet/IP, Profinet ?
Hi Garrett,
Thanks for reply, kindly address following query-
Can we implement MRP redundancy with Modbus TCP/IP protocol on AMIC110?
Also, Is seperate CPU is required for our application? i.e. AMIC for Industrial ethernet protocol and our application on other CPU?