Other Parts Discussed in Thread: THS8200
hi:
I want to see splash screen when my borad is power on,so i have to
port i2c driver ,ths8200 driver, vpbe and osd driver to ubl programer(Iit is
easyer to debug in ccs3.3 envirment than debug uboot),and i have writed down
the vpbe and osd registers values when linux is booting up if i can see svga
pictures, then i set these values in ubl programmer for relative registers. but
when i port the i2c driver from uboot1.2.0 to ubl programmer,I cann't make the
ths8200 work,it seem the i2c driver didn't work well. I am just refering the
file dm355_evm.c in uboot1.2.0,it support some usefule functions just as
I2C_init(),I2C_write(),I2C_read ()...,and it support communication with
msp430.Is it different with ths8200 in i2c communication ? thans a lot!