This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

preview engine of DM365?



Hi, 

there is no so called preview engine in DM365 documents, while DM357 and  644x have such special name in their datasheet. it seems there is no difference among these product on this aspect. isn't DM365 not designed for high-speed preview? From my understanding, if Bayer RAW data is converted into YUV, then it can be displayed on popular device, such TV or specific LCD. 

I'm right? for preview mode,

1. Bayer RAW data is converted to YUV 422 into SDRAM;

2. VPBE read data from SDRAM;

3. display. 

write and read SDRAM can not be at same time, they do it at lagged CLK?

For resize, when it is resized to 1280x768, then if we need to zoom 1:1, we crop image size of 1280x768 from full size. how to crop operation? How does DM365 support pan & tilt?

 

Thanks,

Brian