Part Number: AM3352
Hello Champions,
I need to double check with you if AM3352 is be able to manage a Full HD 1080p 24bpp @ 30fps . Don't need any graph acceleration, need "only" to play Video on a 10inch display.
Standing to DS , AM3352 can manage up to 2048x2048 24bpp @ 30fps ( 126Mhz pixel clock: if I well understood LCD_DATA is sampled only on one edge of LCD_PCLK ) -> Memory bandwidth should be 360MB/s compatible with any DDRx supported .
In my case : 1080x1920 x 24bpp x 30fps I should need a 62Mhz pixel clock and 188MB/s memory bandwidth , well covered my AM3352's specs .
Are my computation right ? can I play a Full HD 30fps Video with Sitara AM3352 ?
There's a correlation between AM3352 clock and the Video capabilities , rephrasing , What is the suggested AM3352 clock speed to manage the Video defined above ?
Thank you,
Paolo