Part Number: LINUXSDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
Tool/software: Linux
Hello
I have an application problem to consult. The chip I used is OMAPL138. I refer to the schematic diagram of peripheral circuit design provided on the official website of TI, and completed the production of two PCB samples. During the sample debugging, it was found that the system failed to start occasionally when it was powered on, with a probability of 10%. This problem was found in both boards. The power on sequence and power-on reset test are normal. Power failure occurs during NAND FLASH or DDR2 self-check.
The error message is as follows:
I2C: READY
DRAM: 128MiB
WARNING: Caches not enabled
NAND: nand_get_flash_type : second ID read did not match 9e, 9e against 01, dc NO NAND FALSH device found!!!
0 MiB
thanks