This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8148: Video codecs support

Part Number: TMS320DM8148


I need more clarification is TMS320DM8148CCYE0 support both Video Encoder, Video Decoder? or it supports one of them (Encoder or Decoder)?

Please, I need your support urgently.

  • Hi Ahmed,

    TMS320DM8148CCYE0 device has Programmable High-Definition Video Image Coprocessing (HDVICP v2) Engine, which can Encode and Decode video.

    The HDVICP2 is a Video Encoder/Decoder hardware accelerator supporting a range of encode, decode, and transcode operations for most major video codec standards. The main video Codec standards supported in hardware are MPEG1/2/4 ASP/SP, H.264 BL/MP/HP, VC-1 SP/MP/AP, RV9/10, AVS-1.0, and ON2 VP6.2/VP7.

    For more info refer to the DM8148 datasheet and TRM.

    Regards,
    Pavel