This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: Error Setting up Main PLL

Part Number: TMS320C6678

Tool/software: Code Composer Studio

Hi,

I'm using C6678 in my custom board.

I'm able to load and run the project successfully but after 2 or 3 times I'm facing the following issue

C66xx_0: GEL Output: Global Default Setup...
C66xx_0: GEL Output: Setup Cache...
C66xx_0: GEL Output: L1P = 32K
C66xx_0: GEL Output: L1D = 32K
C66xx_0: GEL Output: L2 = ALL SRAM
C66xx_0: GEL Output: Setup Cache... Done.
C66xx_0: GEL Output: Main PLL (PLL1) Setup ...
C66xx_0: GEL Output: PLL not in Bypass, Enable BYPASS in the PLL Controller...
C66xx_0: GEL Output: PLL1 Setup for DSP @ 640.0 MHz.
C66xx_0: GEL Output: SYSCLK2 = 213.333328 MHz, SYSCLK5 = 128.0 MHz.
C66xx_0: GEL Output: SYSCLK8 = 10.0 MHz.
C66xx_0: GEL Output: PLL1 Setup... Done.
C66xx_0: GEL Output: DSP core #66 cannot set PSC.
C66xx_0: GEL Output: PA PLL (PLL3) Setup ...
C66xx_0: GEL Output: DSP core #66 cannot set PA PLL
C66xx_0: GEL Output: DDR3 PLL (PLL2) Setup ...
C66xx_0: GEL Output: DSP core #66 cannot set DDR3 PLL
C66xx_0: GEL Output: DDR begin (1333 auto)
C66xx_0: GEL Output: XMC Setup ... Done
C66xx_0: GEL Output:
DDR3 initialization is complete.
C66xx_0: GEL Output: DDR done
C66xx_0: GEL Output: DDR3 memory test... Started
C66xx_0: GEL Output: DDR3 memory test... Failed
C66xx_0: GEL Output: Main PLL (PLL1) Setup ...
C66xx_0: GEL Output: DSP core #66 cannot set PLL1.
C66xx_0: GEL Output: Error in Setting up main PLL, please power cycle the board and re-run Global Default Setup...
Global_Default_Setup() cannot be evaluated.
Evaluation canceledC66xx_0: Power Failure on Target CPU
C66xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

could you please help me to resolve the issue.

Thank you,

Mounika

  • Hi,

    Can you elaborate on the conditions under which you see this error? I.e. are you loading CCS project, are you just connecting to the board to start a debug session, etc...
    Also do you use external Jtag emulator or do you have one built in your board? Can you try with different emulator?

    Best Regards,
    Yordan
  • Hi,

    I'm Loading CCS project to the target using external Jtag emulator. This emulator is working fine since we used it in previous projects.

    I'm facing this issue after loading project to the target after 2 to 3 times without powering off the board.

    And we are facing I2C issue also in which DSP is not sending I2C clk to the slave on SCL

    Thanks,
    Mounika
  • Hi,

    As far as I know, you should use the CPU reset option in ccs (note that this does not power off the board) when loading the same project multiple times on the CPU:
    Can you try this and see if the problem will persist?

    Best Regards,
    Yordan