Part Number: AM3352
Other Parts Discussed in Thread: TPS65910, TPS2065
Tool/software: Linux
Hello, TI experts
Previously SDK01.00.00.03 runs on an am335x-gpevm similar custom board. Everything seems fine include USB1_DRVVBUS. But when SDK04.02.00.09 runs on the same board, USB1_DRVVBUS keeps low on kernel booting. Something I need to say is that the USB power part is different from am335x-gpevm.
- USB device is a 4G modem which connects to USB1, but it is not powered by VDD3_SMPS which comes from SW3 pin of TPS65910. It is powered by +3.6V comes across a MOSFET TPS2065
- USB1_VBUS connect to VDD3_SMPS using 1.2Kohm resistor.
In this condition, I can not see any activity on AM335X_USB1_DRVVBUS pin on SDK04.02.00.09, but can get high level on SDK01.00.00.03. Any advice about this?
Best Regards
Yang