Part Number: TMS320C6657
Other Parts Discussed in Thread: SYSBIOS
Hi,
I get the following error message when trying to run a 'clean' build of the NDK 3.40.01.01. I'm building under windows. XDC version is 3.50.0..24.
C:\work\ndk_3_40_01_01>gmake -f ndk.mak clean
cleaning ndk packages ...
C:\ti\xdctools_3_50_08_24_core\bin\stderr.exe: can't execute 'echo "making" "clean:" "because:" "Invalid" "argument" "C:\ti\xdctools_3_50_08_24_core\bin\stderr.exe:" "can't" "execute" "'date" "'" "(exit" "status" "=" "-1)" "..." ' (exit status = -1) because: Invalid argument
xdctools_3_50_08_24_core\gmake.exe: *** [_startime] Error 255
gmake: *** [clean] Error 2
Any help would be appreciated.
JIm
The ndk.make file contents are:
#
# ======== ndk.mak ========
#
#
# Where to install/stage the packages
# Typically this would point to the devkit location
#
DESTDIR ?= /buildOutput
prefix ?= /
docdir ?= /docs/ndk
packagesdir ?= /packages
# USER STEP: user must define below path to xdc installation
# Set up dependencies
XDC_INSTALL_DIR ?= C:/ti/xdctools_3_50_08_24_core
SYSBIOS_INSTALL_DIR ?= C:/ti/bios_6_73_01_01
NS_INSTALL_DIR ?= C:/ti/ns_2_40_01_02
# Optional: Set this to enable MBEDTLS-enabled SlNetIf libraries
# (not all devices support this yet)
MBEDTLS_INSTALL_DIR ?=
#
# Set location of various cgtools
# These variables can be set here or on the command line.
#
# USER STEP: user must define below paths to compilers
ti.targets.elf.C66 ?= C:/ti/ti-cgt-c6000_8.2.2/bin
ti.targets.elf.C66_big_endian ?=
ti.targets.elf.C674 ?=
ti.targets.arm.elf.Arm9 ?=
ti.targets.arm.elf.A8F ?=
ti.targets.arm.elf.A8Fnv ?=
ti.targets.arm.elf.M3 ?=
ti.targets.arm.elf.M4 ?=
ti.targets.arm.elf.M4F ?=
ti.targets.arm.elf.R5F ?=
gnu.targets.arm.M3 ?=
gnu.targets.arm.M4 ?=
gnu.targets.arm.M4F ?=
gnu.targets.arm.A8F ?=
gnu.targets.arm.A9F ?=
gnu.targets.arm.A15F ?=
iar.targets.arm.M3 ?=
iar.targets.arm.M4F ?=
iar.targets.arm.M4 ?=
# Set BUILDMINSTACK to 1 to only build base stack libraries (stk.a* and stk6.a*)
BUILDMINSTACK ?= 0
# Derive POSIX location from SYSBIOS
TIPOSIX_REPO ?= $(SYSBIOS_INSTALL_DIR)/packages
#
# Set XDCARGS to some of the variables above. XDCARGS are passed
# to the XDC build engine... which will load ndk.bld... which will
# extract these variables and use them to determine what to build and which
# toolchains to use.
#
# Note that not all of these variables need to be set to something valid.
# Unfortunately, since these vars are unconditionally assigned, your build line
# will be longer and more noisy than necessary
#
# Some background is here:
# rtsc.eclipse.org/.../Command_-_xdc
#
XDCARGS= \
ti.targets.arm.elf.Arm9=\"$(ti.targets.arm.elf.Arm9)\" \
ti.targets.arm.elf.A8F=\"$(ti.targets.arm.elf.A8F)\" \
ti.targets.arm.elf.A8Fnv=\"$(ti.targets.arm.elf.A8Fnv)\" \
ti.targets.arm.elf.M3=\"$(ti.targets.arm.elf.M3)\" \
ti.targets.arm.elf.M4=\"$(ti.targets.arm.elf.M4)\" \
ti.targets.arm.elf.M4F=\"$(ti.targets.arm.elf.M4F)\" \
ti.targets.arm.elf.R5F=\"$(ti.targets.arm.elf.R5F)\" \
ti.targets.elf.C66=\"$(ti.targets.elf.C66)\" \
ti.targets.elf.C66_big_endian=\"$(ti.targets.elf.C66_big_endian)\" \
ti.targets.elf.C674=\"$(ti.targets.elf.C674)\" \
gnu.targets.arm.M3=\"$(gnu.targets.arm.M3)\" \
gnu.targets.arm.M4=\"$(gnu.targets.arm.M4)\" \
gnu.targets.arm.M4F=\"$(gnu.targets.arm.M4F)\" \
gnu.targets.arm.A8F=\"$(gnu.targets.arm.A8F)\" \
gnu.targets.arm.A9F=\"$(gnu.targets.arm.A9F)\" \
gnu.targets.arm.A15F=\"$(gnu.targets.arm.A15F)\" \
iar.targets.arm.M3=\"$(iar.targets.arm.M3)\" \
iar.targets.arm.M4F=\"$(iar.targets.arm.M4F)\" \
iar.targets.arm.M4=\"$(iar.targets.arm.M4)\" \
BUILDMINSTACK=\"$(BUILDMINSTACK)\" \
TIPOSIX_REPO=\"$(TIPOSIX_REPO)\" \
MBEDTLS_INSTALL_DIR=$(MBEDTLS_INSTALL_DIR) \
NS_INSTALL_DIR=\"$(NS_INSTALL_DIR)\"
#
# Set XDCPATH to contain necessary repositories.
#
XDCPATH = $(SYSBIOS_INSTALL_DIR)/packages;
export XDCPATH
#
# Set XDCOPTIONS. Use -v for a verbose build.
#
XDCOPTIONS=v
export XDCOPTIONS
j = 8
#
# Set XDC executable command
# Note that XDCBUILDCFG points to the ndk.bld file which uses
# the arguments specified by XDCARGS
#
XDC = $(XDC_INSTALL_DIR)/xdc -j $(j) XDCARGS="$(XDCARGS)" XDCBUILDCFG=./ndk.bld
######################################################
## Shouldnt have to modify anything below this line ##
######################################################
all:
@ echo building ndk packages ...
@ $(XDC) -Pr ./packages
clean:
@ echo cleaning ndk packages ...
@ $(XDC) clean -Pr ./packages
install-packages:
@ echo installing ndk packages to $(DESTDIR) ...
@ mkdir -p $(DESTDIR)/$(prefix)/$(docdir)
@ cp -rf $(wildcard ndk_*_ReleaseNotes.html) docs/* $(DESTDIR)/$(prefix)/$(docdir)
@ mkdir -p $(DESTDIR)/$(prefix)/$(packagesdir)
@ cp -rf packages/* $(DESTDIR)/$(prefix)/$(packagesdir)