Part Number: AM6548
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
I took new release of PDK(1_0_4) and Processor SDK(5_03_00_07). I followed the "can-eth-gateway demo" steps mentioned in :"http://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_examples_demos.html#can-eth-gatway-demo
I have trouble running the demo,
--> Not able to Ping 192.168.1.4 from PC 192.168.1.20
here are few points which are not clear :
1. In "AM65xx IDK" which ethernet port is used for this DEMO, I am connecting on RJ45 named "MCU ETHERNET".
2. In Documentation link above Chapter 9.15.8.5, Point 6 : Load the System firmware as specified in SCICLIENT documentation, Can you please provide the link describing this step . Also if this step is required to RUN the demo?
3. In case PEAK CAN tool is not available, Is it possible to reduce the CAN baud rate to 500Kbps/2Mbps?
4. Flowing error message comes when pause the Program in CCS :
MCU_PULSAR_Cortex_R5_0: Trouble Halting Target CPU: (Error -2062 @ 0x136) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.1.0.00007)
In case some more information helping this topic would be grateful.
Thanks and Regards
Avinash