Part Number: AM3358
Tool/software: Linux
Hi,
I am recently working AM3358 base custom board and custom Linux SDK.
I have followed all the process to create Linux SDK image from the prebuilt image as mention this web:
But I m facing problem in booting process as it's not detecting SD card. I got to know after reading many threads that there is detect GPIO pin for SD detection (in my case :SPI0_CS1(GPIO_6)).
When I make that pin low manually in my custom board, its detect SD card and start booting and everything will work fine.
So How do I Configure that pin so it detects SD card directly?
I know there is some configuration need to do that ignore detection process and start directly.
please help me out.
Thanks in advance