This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TDA3XEVM: Tda3x

Part Number: TDA3XEVM

Tool/software: WEBENCH® Design Tools

Hi,Guys:

Can someone tell me how to set the "Anti-Aliasing" in tda3x because when we look at the videos,the edge looks like "Aliasing".

By the way,the video of ours is infrared,is there any thing we can do to make the picture better? Thanks!

Chen

  • Chen,

    Can you provide an image or video showing the issue?

    Thanks,

    Kyle

  • Also, can you give a summary of the overall dataflow (input via VIN?, output to VOUT?) and processing?

    Thanks,
    KYle
  • HI,KYle:

    This is the dataflow in our porgram.

  • Hi,Kyle:

    please see below the vedio.The output of our vedio is 384*288 and the monitor is SP-17L CCTV LCD MONITOR.

    The edge of the video is fuzzy.So how to improve the quality?

    Another question is about Polyphase FIR.I check that in the path" C:\PROCESSOR_SDK_VISION_03_03_00_00\ti_components\drivers\pdk_01_09_00_17\packages\ti\drv\vps\src\vpslib\hal\src\vpshal_dssDispcPipeTda3xx.c" there is  a variable "gDispcCoefUpScale" looks like the coefficients for the Polyphase FIR.My question is how to set the value of the gDispcCoefUpScale  to get rid of the high frequency components of the image bacause I think maybe the fuzzy edge is caused by some high frequency noise?Thanks.

  • Hi Chen,

    Please look into the GRPx pipe line of display subsystem, it has anti-aliasing feature..

    Rgds,
    Brijesh