Hello,
I have a custom PRGB to LVDS daughtercard on my DM355 EVM driving a 1280x768 LCD. I supply a 74.25MHz clock from the daughtercard. I've developed a similar daughtercard for the DM6446 and was able to get quite good quality video. However, on the DM355 I'm seeing noise that has me stumped.
Please excuse the poor quality of the attached photo, but it gets the idea across. In the photo, I am using the decode demo to display a test pattern that I captured using the encode demo. The displayed image and the captured image are both at 720x480 resolution. The video looks fine on the standard NTSC output, with and without the on screen display.
However, when I switch to PRGB output, using the driver code developed for my DM6446 project, the image is quite noisy. In the photo, the worst of the noise is in the top half of the image. The decode demo OSD is not displayed, but the OSD is active and squeezed into the top half of the image on purpose for debugging. When the OSD is disabled completely, the noise is much less severe, as it is in the bottom half of the photo.
What am I seeing here? Anyone have any experience with similar noise?
Thanks!
-Vim