This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5748: PCIe interface

Part Number: AM5748

Tool/software: Linux

Hi champs

I am having an issue with PCIe on my board. i get the below 

I also started looking at The LTSSM_STATE from the PCIECTRL_TI_CONF_DEVICE_CMD. It looks like go from 0 (DETECT_QUITE) to 1 (DETECT_ACT) to 9 (CFG_LANENUM_WAIT), eventually back to 5 (PRE_DETECT_QUIET) and then back to 9 (CFG_LANENUM_WAIT). 

Any ideas as to what is going on?

Also when do i have to take the peripheral that is connected to the AM574x PCIe  out of reset?

Thanks