Part Number: AM5728
Tool/software: Linux
Hi,
I'm using ,
Hardware : TMDSEVM572X AM572x General purpose Evaluation Module
SDK : ti-processor-sdk-linux-am57xx-evm-05.03.00.07-Linux-x86-Install.bin
i want to compile individual device tree overlay files and load them into the kernel after the boot up..
to achieve the same , as per my understanding , Cape manager, slots and overlay files are required and echo command is used for loading...
Kindly please help us achieve the same in am57xx .
Thanks.