This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Failed to boot from nfs with am335x board. ti-processor-sdk-linux-am335x-evm-05.02.00.10

Tool/software: Linux

Hello everyone,

I can't boot from NFS.

My NFS server is working. And I can download files with nfs in u-boot. But I can't boot linux from nfs.

Here is the booting logs:

Could anyone kindly help me out?

Thank you very much!

  • Hi,

    Could you please capture the entire boot log and attach it as a file to your post? I'm sorry, the screen captures are lacking too much information and are too hard to read in order to be able to provide good help.

    Thank you.
  • Hi!

    Thank you for reply!

    After some probe and debug, I have some new information:

    I've turn on the NAND_DEBUG,and the boot log is the following:

    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.14.79-gbde58ab01e (zlh@zlh-ThinkPad-E460) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #7 PREEMPT Mon May 6 11:29:15 CST 2019
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] OF: fdt: Machine model: TI AM335x EVM-SK
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 48 MiB at 0x8a800000
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] AM335X ES2.1 (sgx neon)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 64960
    [    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.1.103:/tftpboot/rootfs/,nolock rw nfsrootdebug
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 197280K/262144K available (8192K kernel code, 321K rwdata, 2556K rodata, 1024K init, 267K bss, 15712K reserved, 49152K cma-reserved, 0K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xff800000   ( 752 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc0900000   (9184 kB)
    [    0.000000]       .init : 0xc0c00000 - 0xc0d00000   (1024 kB)
    [    0.000000]       .data : 0xc0d00000 - 0xc0d50480   ( 322 kB)
    [    0.000000]        .bss : 0xc0d50480 - 0xc0d932fc   ( 268 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Tasks RCU enabled.
    [    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [    0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
    [    0.000032] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
    [    0.000042] OMAP clocksource: timer1 at 24000000 Hz
    [    0.000190] timer_probe: no matching timers found
    [    0.000394] Console: colour dummy device 80x30
    [    0.000419] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.000426] This ensures that you still see kernel messages. Please
    [    0.000431] update your kernel commandline.
    [    0.000460] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
    [    0.089226] pid_max: default: 32768 minimum: 301
    [    0.089397] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.089411] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.090154] CPU: Testing write buffer coherency: ok
    [    0.090219] CPU0: Spectre v2: using BPIALL workaround
    [    0.090888] Setting up static identity map for 0x80100000 - 0x80100060
    [    0.091037] Hierarchical SRCU implementation.
    [    0.091354] EFI services will not be available.
    [    0.092574] devtmpfs: initialized
    [    0.099547] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
    [    0.099998] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    0.100297] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.100320] futex hash table entries: 256 (order: -1, 3072 bytes)
    [    0.103835] pinctrl core: initialized pinctrl subsystem
    [    0.104550] DMI not present or invalid.
    [    0.104957] NET: Registered protocol family 16
    [    0.107072] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.119612] omap_hwmod: debugss: _wait_target_disable failed
    [    0.171742] cpuidle: using governor ladder
    [    0.171774] cpuidle: using governor menu
    [    0.175785] OMAP GPIO hardware version 0.1
    [    0.183458] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe
    [    0.185300] No ATAGs?
    [    0.185314] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.197424] edma 49000000.edma: TI EDMA DMA engine driver
    [    0.201124] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
    [    0.201256] media: Linux media interface: v0.10
    [    0.201303] Linux video capture interface: v2.00
    [    0.201401] pps_core: LinuxPPS API ver. 1 registered
    [    0.201409] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.201430] PTP clock support registered
    [    0.201461] EDAC MC: Ver: 3.0.0
    [    0.201922] dmi: Firmware registration failed.
    [    0.202323] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [    0.202641] Advanced Linux Sound Architecture Driver Initialized.
    [    0.203786] clocksource: Switched to clocksource timer1
    [    0.211370] NET: Registered protocol family 2
    [    0.212071] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.212103] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.212126] TCP: Hash tables configured (established 2048 bind 2048)
    [    0.212229] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.212246] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.212415] NET: Registered protocol family 1
    [    0.212944] RPC: Registered named UNIX socket transport module.
    [    0.212957] RPC: Registered udp transport module.
    [    0.212964] RPC: Registered tcp transport module.
    [    0.212969] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.213965] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    0.214118] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
    [    0.215500] workingset: timestamp_bits=14 max_order=16 bucket_order=2
    [    0.219339] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.220150] NFS: Registering the id_resolver key type
    [    0.220200] Key type id_resolver registered
    [    0.220207] Key type id_legacy registered
    [    0.220223] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.220257] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.222217] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.222236] io scheduler noop registered
    [    0.222244] io scheduler deadline registered
    [    0.222450] io scheduler cfq registered (default)
    [    0.222459] io scheduler mq-deadline registered
    [    0.222466] io scheduler kyber registered
    [    0.223594] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
    [    0.269891] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.272879] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
    [    0.915346] console [ttyS0] enabled
    [    0.919905] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250
    [    0.929676] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 32, base_baud = 3000000) is a 8250
    [    0.939359] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 33, base_baud = 3000000) is a 8250
    [    0.949041] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 34, base_baud = 3000000) is a 8250
    [    0.959498] omap_rng 48310000.rng: Random Number Generator ver. 20
    [    0.977531] brd: module loaded
    [    0.987130] loop: module loaded
    [    0.992492] libphy: Fixed MDIO Bus: probed
    [    1.063871] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
    [    1.071572] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
    [    1.079758] libphy: 4a101000.mdio: probed
    [    1.083903] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet
    [    1.093165] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 ethernet
    [    1.103359] cpsw 4a100000.ethernet: Detected MACID = 60:64:05:f0:af:1f
    [    1.110234] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
    [    1.116682] cpsw 4a100000.ethernet: ALE Table size 1024
    [    1.121968] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
    [    1.129980] cpsw 4a100000.ethernet: cpsw: Detected MACID = 60:64:05:f0:af:21
    [    1.138295] i2c /dev entries driver
    [    1.142226] IR NEC protocol handler initialized
    [    1.146852] IR RC5(x/sz) protocol handler initialized
    [    1.151923] IR RC6 protocol handler initialized
    [    1.156482] IR JVC protocol handler initialized
    [    1.161027] IR Sony protocol handler initialized
    [    1.165671] IR SANYO protocol handler initialized
    [    1.170391] IR Sharp protocol handler initialized
    [    1.175122] IR MCE Keyboard/mouse protocol handler initialized
    [    1.180975] IR XMP protocol handler initialized
    [    1.187111] cpuidle: enable-method property 'ti,am3352' found operations
    [    1.194274] sdhci: Secure Digital Host Controller Interface driver
    [    1.200484] sdhci: Copyright(c) Pierre Ossman
    [    1.205412] omap_hsmmc 48060000.mmc: Got CD GPIO
    [    1.210838] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.217667] ledtrig-cpu: registered to indicate activity on CPUs
    [    1.226474] ipip: IPv4 and MPLS over IPv4 tunneling driver
    [    1.232550] gre: GRE over IPv4 demultiplexor driver
    [    1.237601] ip_gre: GRE over IPv4 tunneling driver
    [    1.244054] NET: Registered protocol family 10
    [    1.250319] Segment Routing with IPv6
    [    1.254213] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    1.260809] NET: Registered protocol family 17
    [    1.265647] Key type dns_resolver registered
    [    1.270138] omap_voltage_late_init: Voltage driver support not added
    [    1.281908] omap-gpmc 50000000.gpmc: GPMC revision 6.0
    [    1.287271] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
    [    1.295270] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0x38
    [    1.301658] nand: Micron MT29F8G08ABABAWP
    [    1.305816] nand: 1024 MiB, SLC, erase size: 512 KiB, page size: 4096, OOB size: 224
    [    1.313648] __trace__ device node: name: elm, type: <NULL>, full name: /ocp/elm@48080000
    [    1.321836] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
    [    1.327320] 10 ofpart partitions found on MTD device omap2-nand.0
    [    1.333439] Creating 10 MTD partitions on "omap2-nand.0":
    [    1.338898] 0x000000000000-0x000000080000 : "NAND.SPL"
    [    1.345141] 0x000000080000-0x000000100000 : "NAND.SPL.backup1"
    [    1.351798] 0x000000100000-0x000000180000 : "NAND.SPL.backup2"
    [    1.358498] 0x000000180000-0x000000200000 : "NAND.SPL.backup3"
    [    1.365200] 0x000000200000-0x000000280000 : "NAND.u-boot-spl-os"
    [    1.371997] 0x000000280000-0x000000380000 : "NAND.u-boot"
    [    1.378273] 0x000000380000-0x000000400000 : "NAND.u-boot-env"
    [    1.384871] 0x000000400000-0x000000480000 : "NAND.u-boot-env.backup1"
    [    1.392091] 0x000000480000-0x000000c80000 : "NAND.kernel"
    [    1.399082] 0x000000c80000-0x00003fc80000 : "NAND.file-system"
    [    1.524068] tps65910 0-002d: No interrupt support, no core IRQ
    [    1.531786] vrtc: supplied by vbat
    [    1.538868] vio: supplied by vbat
    [    1.543584] vdd1: supplied by vbat
    [    1.548776] vdd2: supplied by vbat
    [    1.553626] random: fast init done
    [    1.558625] vdig1: supplied by vbat
    [    1.563397] vdig2: supplied by vbat
    [    1.568230] vpll: supplied by vbat
    [    1.572933] vdac: supplied by vbat
    [    1.577666] vaux1: supplied by vbat
    [    1.582446] vaux2: supplied by vbat
    [    1.587263] vaux33: supplied by vbat
    [    1.592141] vmmc: supplied by vbat
    [    1.596871] vbb: supplied by vbat
    [    1.601856] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
    [    1.609572] omap_hsmmc 48060000.mmc: Got CD GPIO
    [    1.675774] hctosys: unable to open rtc device (rtc0)
    [    1.681876] lis3_reg: disabling
    [    1.687119] ALSA device list:
    [    1.692146]   No soundcards found.
    [    1.696820] Root-NFS: nfsroot=/tftpboot/rootfs/,nolock
    [    1.703060] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [    1.712326] NFS:   parsing nfs mount option 'vers=2'
    [    1.718487] NFS:   parsing nfs mount option 'udp'
    [    1.723211] NFS:   parsing nfs mount option 'rsize=4096'
    [    1.728597] NFS:   parsing nfs mount option 'wsize=4096'
    [    1.733964] NFS:   parsing nfs mount option 'nolock'
    [    1.738948] NFS:   parsing nfs mount option 'nolock'
    [    1.743944] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [    1.749990] NFS: MNTPATH: '/tftpboot/rootfs/'
    [    1.754403] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [    1.762040] NFS: failed to create MNT RPC client, status=-101
    [    1.767916] NFS: unable to mount server 192.168.1.103, error -101
    [    1.774109] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [    6.806729] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [    6.815969] NFS:   parsing nfs mount option 'vers=2'
    [    6.821003] NFS:   parsing nfs mount option 'udp'
    [    6.825791] NFS:   parsing nfs mount option 'rsize=4096'
    [    6.831156] NFS:   parsing nfs mount option 'wsize=4096'
    [    6.837017] NFS:   parsing nfs mount option 'nolock'
    [    6.842004] NFS:   parsing nfs mount option 'nolock'
    [    6.847007] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [    6.853049] NFS: MNTPATH: '/tftpboot/rootfs/'
    [    6.857459] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [    6.864789] NFS: failed to create MNT RPC client, status=-101
    [    6.870568] NFS: unable to mount server 192.168.1.103, error -101
    [    6.876772] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [   17.124675] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [   17.134152] NFS:   parsing nfs mount option 'vers=2'
    [   17.139388] NFS:   parsing nfs mount option 'udp'
    [   17.144189] NFS:   parsing nfs mount option 'rsize=4096'
    [   17.149555] NFS:   parsing nfs mount option 'wsize=4096'
    [   17.155124] NFS:   parsing nfs mount option 'nolock'
    [   17.160282] NFS:   parsing nfs mount option 'nolock'
    [   17.165282] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [   17.171323] NFS: MNTPATH: '/tftpboot/rootfs/'
    [   17.175726] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [   17.182971] NFS: failed to create MNT RPC client, status=-101
    [   17.188811] NFS: unable to mount server 192.168.1.103, error -101
    [   17.194990] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [   37.606701] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [   37.615934] NFS:   parsing nfs mount option 'vers=2'
    [   37.620965] NFS:   parsing nfs mount option 'udp'
    [   37.625755] NFS:   parsing nfs mount option 'rsize=4096'
    [   37.631121] NFS:   parsing nfs mount option 'wsize=4096'
    [   37.636949] NFS:   parsing nfs mount option 'nolock'
    [   37.641938] NFS:   parsing nfs mount option 'nolock'
    [   37.646940] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [   37.652981] NFS: MNTPATH: '/tftpboot/rootfs/'
    [   37.657387] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [   37.664639] NFS: failed to create MNT RPC client, status=-101
    [   37.670414] NFS: unable to mount server 192.168.1.103, error -101
    [   37.676607] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [   68.326708] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [   68.335939] NFS:   parsing nfs mount option 'vers=2'
    [   68.340968] NFS:   parsing nfs mount option 'udp'
    [   68.345755] NFS:   parsing nfs mount option 'rsize=4096'
    [   68.351119] NFS:   parsing nfs mount option 'wsize=4096'
    [   68.356944] NFS:   parsing nfs mount option 'nolock'
    [   68.361932] NFS:   parsing nfs mount option 'nolock'
    [   68.366935] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [   68.372975] NFS: MNTPATH: '/tftpboot/rootfs/'
    [   68.377383] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [   68.384615] NFS: failed to create MNT RPC client, status=-101
    [   68.390391] NFS: unable to mount server 192.168.1.103, error -101
    [   68.396581] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [   99.046698] NFS: nfs mount opts='vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103'
    [   99.055929] NFS:   parsing nfs mount option 'vers=2'
    [   99.060957] NFS:   parsing nfs mount option 'udp'
    [   99.065755] NFS:   parsing nfs mount option 'rsize=4096'
    [   99.071121] NFS:   parsing nfs mount option 'wsize=4096'
    [   99.076954] NFS:   parsing nfs mount option 'nolock'
    [   99.081942] NFS:   parsing nfs mount option 'nolock'
    [   99.086941] NFS:   parsing nfs mount option 'addr=192.168.1.103'
    [   99.092981] NFS: MNTPATH: '/tftpboot/rootfs/'
    [   99.097390] NFS: sending MNT request for 192.168.1.103:/tftpboot/rootfs/
    [   99.104622] NFS: failed to create MNT RPC client, status=-101
    [   99.110397] NFS: unable to mount server 192.168.1.103, error -101
    [   99.116592] __trace__ err: -101, name: 192.168.1.103:/tftpboot/rootfs/, flags: 8000, root_mount_data: vers=2,udp,rsize=4096,wsize=4096,nolock,nolock,addr=192.168.1.103
    [   99.131657] VFS: Unable to mount root fs via NFS, trying floppy.
    [   99.138234] VFS: Cannot open root device "nfs" or unknown-block(2,0): error -6
    [   99.145595] Please append a correct "root=" boot option; here are the available partitions:
    [   99.154033] 0100           65536 ram0 
    [   99.154039]  (driver?)
    [   99.160167] 0101           65536 ram1 
    [   99.160170]  (driver?)
    [   99.166361] 0102           65536 ram2 
    [   99.166365]  (driver?)
    [   99.172490] 0103           65536 ram3 
    [   99.172493]  (driver?)
    [   99.178665] 0104           65536 ram4 
    [   99.178668]  (driver?)
    [   99.184822] 0105           65536 ram5 
    [   99.184825]  (driver?)
    [   99.190950] 0106           65536 ram6 
    [   99.190953]  (driver?)                                                                                             
    [   99.197107] 0107           65536 ram7                                                                              
    [   99.197110]  (driver?)                                                                                             
    [   99.203235] 0108           65536 ram8                                                                              
    [   99.203238]  (driver?)                                                                                             
    [   99.209377] 0109           65536 ram9 
    [   99.209380]  (driver?)
    [   99.215531] 010a           65536 ram10                                                                             
    [   99.215534]  (driver?)                                                                                             
    [   99.221747] 010b           65536 ram11                                                                             
    [   99.221750]  (driver?)                                                                                             
    [   99.227975] 010c           65536 ram12                                                                             
    [   99.227978]  (driver?)
    [   99.234203] 010d           65536 ram13 
    [   99.234206]  (driver?)
    [   99.240418] 010e           65536 ram14 
    [   99.240421]  (driver?)
    [   99.246659] 010f           65536 ram15 
    [   99.246662]  (driver?)
    [   99.252882] 1f00             512 mtdblock0 
    [   99.252885]  (driver?)
    [   99.259462] 1f01             512 mtdblock1 
    [   99.259465]  (driver?)
    [   99.266051] 1f02             512 mtdblock2 
    [   99.266055]  (driver?)
    [   99.272616] 1f03             512 mtdblock3 
    [   99.272620]  (driver?)
    [   99.279196] 1f04             512 mtdblock4 
    [   99.279199]  (driver?)
    [   99.285773] 1f05            1024 mtdblock5 
    [   99.285776]  (driver?)
    [   99.292338] 1f06             512 mtdblock6 
    [   99.292341]  (driver?)
    [   99.298932] 1f07             512 mtdblock7 
    [   99.298936]  (driver?)
    [   99.305512] 1f08            8192 mtdblock8 
    [   99.305515]  (driver?)
    [   99.312076] 1f09         1032192 mtdblock9 
    [   99.312079]  (driver?)
    [   99.318657] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
    [   99.326967] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

    I boot from nand and tried to mount nfs filesystem, failed: svc: failed to register lockdv1 RPC service (errno 111).

    Then I searched the web, it told me to add a "nolock" option. It did work!

    But there is nolock option in the kernel parameter u-boot provided. so puzzled.

    Thank you very much!

  • Hi,

    Just checking in to see if you've found a solution to this problem? If not, can you provide an update on your current status?

    Thanks.
  • Hi, 

    I have not found any solution yet, and the status is just remained. As a workaround I've flashed the images into nand and boot from it. Then mount nfs file system after linux is up. That works for application development.

    If you have any ideal, please let me known.

    Thank you very much.

  • Hi,

    I'm sorry, the only thing that I've come up with in my research is to play with NFS versions by trying to make sure what is on the target and the host is compatible.

    I hope this helps.