This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reference schematic

Other Parts Discussed in Thread: TMS320C6416

Hi,

When I download SPRC138 and unzip the document, there's only an OLB file not orcad schematic file. Could you tell what's the matter?

  • Hi user5988799,

    Could you post a link to the page where downloading SPRC138. Which board schematic you are looking for?

    Regards,
    Tsvetolin Shulev
  • Hi Shulev,

    Here's the link: for TMS320C6416 schematic for reference

    www.ti.com/.../getliterature.tsp

  • Hi,

    Sorry for the delay.

    The Schematics for the DSK6416 (in PDF format) are located at c6000.spectrumdigital.com/.../

    CAD/CAE symbols can be converted from the universal .bxl format to Cadence format with UltraLibrarian: www.ti.com/.../sprc137

    According to the C6416 Hardware Designer's Resource Guide (SPRA943B), the OLB file contains the schematic symbols and layout footprints that can be used to create schematics. I would try first with the UltraLibrarian output, however.

    I did not open the .olb file. Are the schematic symbols present?

    SPRA943B:
    2.3 Schematics
    This section includes ORCAD symbols that should help in schematic generation. The method that we have chosen to provide the ORCAD symbols is a multi-section package further defined as a heterogeneous package. That is to say that the logical parts in the package have different graphics, numbers of pins, or properties. In the case of the TMS320C6416 DSP, we have created an ORCAD library that contains 14 parts. This allows the schematic designer to easily connect the various parts on separate schematic pages and yet retain the same reference
    designator for the part across all schematic pages. The list below describes which pins are assigned to a part.

    Several peripherals use multiplexed pins. In cases in which pins are shared, one peripheral will be enabled and the other will be disabled. Please refer to the data sheet for more information concerning multiplexed pins.

    You can find the ORCAD symbols here:
    TMS320C6416 Orcad Symbol (SPRC138)

    Regards,
    Mark