This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H: How to connect two EVMK2H board for PCIe example?

Part Number: EVMK2H

Hi there,

I am trying to run the PCIe example included with the processor SDK for the K2H EVM. I have two EVMK2H demo boards, and two of the RTM Break-out cards for the Keystone II EVM. Once I have built and loaded the PCIe demo on each board, how do I connect the two boards together physically so they can talk over PCIe?

I see from the Advantech documentation for the demo board, that two PCIe lanes connect directly to the AMC edge connector. Page 29 here: http://wfcache.advantech.com/www/support/TI-EVM/download/XTCIEVMK2X_Technical_Reference_Manual_Rev1_0.pdf

Do I need a double-sided female AMC connector?

Do I need an AMC to PCIe Adapter Card, like the following: http://www.ti.com/tool/TMDXEVMPCI#0

Or can I somehow make use of the RTM break-out card that we have already bought?

Please advise as to how to proceed. The PCIe example in the SDK simply says "Connect the two boards together" but does not state how.

Thanks,
Andre