This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA72XEVM: ### XDC ASSERT - ERROR CALLBACK START ###

Part Number: DRA72XEVM

Tool/software: Linux

Hi TI team,

We are using PVSDK_03_04 SDK in DRA72XEVM board.

While running apps.out getting ### XDC ASSERT - ERROR CALLBACK START ###
[ 50.784428] DMA: Module install successful, device major num = 242
[ 50.793642] DRV: Module install successful
[HOST] OSA: MEM: 0: Mapped 0xa0100000 to 0xb6993000 of size 0x00100000
[HOST] OSA: MEM: 1: Mapped 0x84203000 to 0xa6f93000 of size 0x0fa00000
[HOST] OSA: MEM: 2: Mapped 0xa0200000 to 0xa6ed3000 of size 0x00040000
[HOST] OSA: MEM: 3: Mapped 0xa02c0000 to 0xa6f13000 of size 0x00080000
[HOST] OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000
[HOST] OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000
[HOST] OSA: HOST Remote Log Shared Memory @ 0xa024f140
[HOST] OSA: DSP1 Remote Log Shared Memory @ 0xa02769e0
SYSTEM: System A15 Init in progress !!!
[HOST] [IPU1-0] 30.936100 s: ***** IPU1_0 Firmware build time 16:47:32 Apr 23 2019
[HOST] [IPU1-0] 30.936283 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[HOST] [IPU1-0] 30.939150 s: SYSTEM: System Common Init in progress !!!
[HOST] [IPU1-0] 30.948362 s: UTILS: CIO: Init Done !!!
[HOST] [IPU1-0] 30.948453 s: SYSTEM: IPC init in progress !!!
[HOST] [IPU1-0] 30.948575 s: SYSTEM: Attaching to [DSP1] ...
[HOST] [IPU1-0] 31.169950 s: SYSTEM: Attaching to [DSP1] ... SUCCESS !!!
[HOST] [IPU1-0] 31.170042 s: SYSTEM: Notify register to [DSP1] line 0, event 15...
[HOST] [IPU1-0] 31.170194 s: SYSTEM: Notify init done !!!
[HOST] [IPU1-0] 31.171933 s: SYSTEM: MsgQ init done !!!
[HOST] [IPU1-0] 31.172878 s: RpmsgInit in progress...
[HOST] [IPU1-0] 31.172970 s: Connection established with HLOS, calling rpmsgInit
[HOST] [IPU1-0] 31.173031 s: rpmsgStartUp 209
[HOST] [IPU1-0] 31.173275 s:
[HOST] [IPU1-0] 31.173305 s: ### XDC ASSERT - ERROR CALLBACK START ###
[HOST] [IPU1-0] 31.173397 s:
[HOST] [IPU1-0] 31.173732 s: assertion failure
[HOST] [IPU1-0] 31.173793 s:
[HOST] [IPU1-0] 31.173854 s: ### XDC ASSERT - ERROR CALLBACK END ###
[HOST] [IPU1-0] 31.173915 s:
[HOST] [DSP1 ] 31.167571 s: ***** DSP1 Firmware build time 16:46:53 Apr 23 2019
[HOST] [DSP1 ] 31.167602 s: *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 750000000 Hz>
[HOST] [DSP1 ] 31.167785 s: SYSTEM: System Common Init in progress !!!
[HOST] [DSP1 ] 31.167968 s: UTILS: CIO: Init Done !!!
[HOST] [DSP1 ] 31.167998 s: SYSTEM: IPC init in progress !!!
[HOST] [DSP1 ] 31.167998 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 31.169950 s: SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!
[HOST] [DSP1 ] 31.169981 s: SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[HOST] [DSP1 ] 31.170011 s: SYSTEM: Notify init done !!!
[HOST] [DSP1 ] 31.170133 s: SYSTEM: MsgQ init done !!!
[HOST] [DSP1 ] 31.170194 s: RpmsgInit in progress...
[HOST] [DSP1 ] 31.170255 s: SYSTEM: IPC init DONE !!!
[HOST] [DSP1 ] 31.170835 s: SYSTEM: System Common Init Done !!!
[HOST] [DSP1 ] 31.170865 s: SYSTEM: System DSP Init in progress !!!
[HOST] [DSP1 ] 31.171018 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[HOST] [DSP1 ] 31.171048 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[HOST] [DSP1 ] 31.171109 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 522056 B (509 KB)
[HOST] [DSP1 ] 31.171140 s: SYSTEM: Initializing Links !!!
[HOST] [DSP1 ] 31.177758 s: SYSTEM: Initializing Links ... DONE !!!
[HOST] [DSP1 ] 31.177819 s: lz4CompDecomp Init
[HOST] [DSP1 ] 31.177850 s: SYSTEM: System DSP Init Done !!!
[HOST] [DSP1 ] 31.199780 s: Connection established with HLOS, calling rpmsgInit
[HOST] [DSP1 ] 31.199810 s: rpmsgStartUp 209
[HOST] [DSP1 ] 31.199871 s:
[HOST] [DSP1 ] 31.199902 s: ### XDC ASSERT - ERROR CALLBACK START ###
[HOST] [DSP1 ] 31.199902 s:
[HOST] [DSP1 ] 31.199993 s: assertion failure
[HOST] [DSP1 ] 31.200024 s:
[HOST] [DSP1 ] 31.200024 s: ### XDC ASSERT - ERROR CALLBACK END ###
[HOST] [DSP1 ] 31.200054 s:

Please help me resolve this issue..

Thanks & Regards,

Sudhi

  • Hi,

    The assert is coming from DSP1.
    So please revert your chnages and check which changes is causing this.
    There is no direct solution of XDC assert.
    After doing any modification please do a clean build.
    Sometime it may happen as the building was not clean.

    Regards,
    Anuj