Part Number: AM5728
Hello
We are using AM5728 in one of our project that need to work from -40 Degree C to 85 Degree C.
But i have found the below in Errata
i925 PCI-Express Gen2 (5.0 GT/s) Operation Not Supported When Operating Junction Temperature Less than 0 Deg C CRITICALITY High DESCRIPTION PCI-Express (PCIe) Gen2 (5.0 GT/s) operation is not supported for operating junction temperatures (Tj) of < 0°C. Limit device operation to PCIe Gen1 (2.5 GT/s) in both Endpoint and Root-Complex configurations when Tj < 0°C. WORKAROUND None REVISIONS IMPACTED SR 2.0, 1.1
So need to ensure that PCie Gen 1 will work till -45 degree C or not?
Regards
Akash Jain