Part Number: AM3352
Hi Team,
Observing failure with following command
ubi part nand0,0 2048;
Processor results in continuous reset with following log
_____________________________________________________________________________________
U-Boot SPL 2016.05-rc3 (Oct 20 2016 - 17:30:33)
Trying to boot from SPI
U-Boot 2016.05-rc3 (Oct 20 2016 - 17:30:33 +0530)
Watchdog enabled
DRAM: 256 MiB
NAND: 256 MiB
SF: Detected S25FL164K with page size 256 Bytes, erase size 64 KiB, total 8 MiB
Press SPACE to abort autoboot in 0 seconds
Booting from nand ...
data abort
pc : [<8ffb7812>] lr : [<8ffb6b79>]
reloc pc : [<8081e812>] lr : [<8081db79>]
sp : 8ef88740 ip : 00000000 fp : 00000028
r10: 0001f000 r9 : 8ef88ee0 r8 : 00000000
r7 : 000000dc r6 : 0001f000 r5 : 8ef90400 r4 : 8f03a940
r3 : 00000000 r2 : 000000da r1 : 8ef90678 r0 : 00000000
Flags: nZCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
_____________________________________________________________________________________
Environment is currently set to -
_____________________________________________________________________________________
=> print
alt2bootcmd=echo BOOTFAILED....; gpio set 46;
altbootcmd=echo booting from recovery images...; run setrecoveryboot; setenv bootfile ${altbootfile}
altbootfile=recovery/zImage
altfdtfile=recovery/beanbag-gateway-am3352.dtb
arch=arm
baudrate=115200
board=beanbag
board_name=beanbag
boot_targets=nand
bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
bootcmd_flasher=echo Booting from TFTP over USB RNDIS ...; setenv autoload no; setenv ethact usb_eth000; fi;
bootcmd_nand=echo Booting from nand ...; run nandargs; dcache on; ubi part nand0,0 2048; ubifsmount t; then bootz ${loadaddr} - ${fdtaddr};else echo WARN: Failed to load boot/${fdtfile}; fi; else echod;
bootcount=1
bootdelay=0
bootfailed=mw 0x44E3E064 0x010002b0; reset;
bootfile=zImage
bootlimit=3
bootm_size=0x10000000
console=ttyO0,115200n8
cpu=armv7
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtfile=beanbag-gateway-am3352.dtb
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadfdt=ubifsload ${fdtaddr} boot/${fdtfile}
loadimage=ubifsload ${loadaddr} boot/${bootfile}
mtddevname=NAND.file-system
mtddevnum=0
mtdids=nand0=nand.0
mtdparts=mtdparts=nand.0:-(NAND.file-system)
nandargs=setenv bootargs console=${console} ${optargs} root=${nandroot} rootfstype=${nandrootfstype}
nandroot=ubi0:beanbag-rootfs rw ubi.mtd=NAND.file-system,2048
nandrootfstype=ubifs rootwait=1
optargs=quiet
partition=nand0,0
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
scriptaddr=0x80000000
setrecoveryboot=mw 0x44E3E064 0x000102b0;
soc=am33xx
stderr=ns16550_serial
stdin=ns16550_serial
stdout=ns16550_serial
vendor=secure
ver=U-Boot 2016.05-rc3 (Oct 20 2016 - 17:30:33 +0530)
Environment size: 1967/65531 bytes
_____________________________________________________________________________________
Any pointers to debug further?