Tool/software: Linux
Hi.
I'm working on porting TIDL_OD Usecase to Linux + BIOS using TDA2xx EVM.
I think the porting operation is almost finished, but the following errors occur during the execution.
// Alg_tidlpreproc status = System_linkCreate(pObj->Alg_tidlpreprocLinkID, &pObj->Alg_tidlpreprocPrm, sizeof(pObj->Alg_tidlpreprocPrm)); UTILS_assert(status == SYSTEM_LINK_STATUS_SOK);
ASSERT (chains_dl_od_priv.c|chains_dl_od_Create|542)
ALG: ERROR: No alg create function specified (algId = 12) !!!
I found the ALG_ID 12 is tidl_preproc. (TIDL_Preproc(A15))
I searched the forum and checked the file in "/src/common/app_init/app_init_a15.c", but it was found.
#include <system_cfg.h> #include <src/rtos/utils_common/include/utils.h> #include <include/link_api/system_common.h> /******************************************************************************* * Function prototypes ******************************************************************************* */ #ifdef ALG_framecopy Int32 AlgorithmLink_FrameCopy_initPlugin(void); #endif #ifdef ALG_safe_framecopy Int32 AlgorithmLink_SafeFrameCopy_initPlugin(void); #endif #ifdef ALG_objectdetection Int32 AlgorithmLink_objectDraw_initPlugin(void); #endif #ifdef ALG_tidl Int32 AlgorithmLink_tidlpreproc_initPlugin(void); Int32 AlgorithmLink_tidlpostproc_initPlugin(Void); #endif /** ******************************************************************************* * * \brief Application init * ******************************************************************************* */ void App_init(void) { /* Algorithms plug in init */ #ifdef ALG_framecopy AlgorithmLink_FrameCopy_initPlugin(); #endif #ifdef ALG_safe_framecopy AlgorithmLink_SafeFrameCopy_initPlugin(); #endif #ifdef ALG_objectdetection AlgorithmLink_objectDraw_initPlugin(); #endif #ifdef ALG_tidl AlgorithmLink_tidlpreproc_initPlugin(); AlgorithmLink_tidlpostproc_initPlugin(); #endif } /** ******************************************************************************* * * \brief Application deinit * ******************************************************************************* */ void App_deInit(void) { /* Algorithms plug in deinit */ } /* Nothing beyond this point */
How can i fix this error?