Tool/software: TI-RTOS
Hi All,
I am working with linux OS on tda2xx board, I want to split the display into 2(in different resolution). In one part I have to display stitched image which is created using sgxfrmcpy link. In second part I have to display one of the input camera view. I found following ways to solve this :
1]Using sgxfrmcpy and 1x2 rendering
I have seen lvds_vip_multi_cam_view_sgx_display usecase in which 4 camera views are shown. Using same concept is is possible to solve above mentioned problem ? I mean is it possible to create 1x2 display(in different resolution or half). If yes then what are the changes for the same.
2] Using DssM2mwb
Can I use DssM2mwb link? and does it supports one part as result from sgxfrmcpy link and other to be a view from any one camera(out of 4 camera's).
Please provide input and suggest an optimal solution from above. And if there is any other way then please share.
Thank you.
Regards,
Salman