This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: PCIe Trouble Detecting

Part Number: AM5728


Tool/software: Linux

Customer has AM5728  in design. Currently they have an issue detecting PCIe bus from a device. PCIe bus is detected at AM5728 okay; however, PCIe bus at the device side is not.

 

The device is out of reset and transmits the PCIe bus constantly to CPU (it is CPU_PCIE_RX) approximately 20ms prior to CPU to scan the PCIe bus once (CPU_PCIE_TX).  The design provides external PCIe 100MHz clock, LP-HCSL output format to both AM5728 and the device.

 

Any suggestion?