This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3359: Which linus SDK/Image is best for SUTARA AM335X STARTER KIT

Part Number: AM3359

Tool/software: Linux

hello

im bot be able to modify the ti arm linux sdk

after modify in kernal and while im save image and load using default image select it will not be loaded in sd card and which one image file is best for stater lit i.e. U-image file or ZImage file

and whits advantage of Ti-Rtos over ti linux sdk and which sdk versiion should i used in official site there in 5.03 sdk version is available but in e2e community there is 8.00 sdk version is available

is anyone have sd card creation using custom sdk then please post snap shot of it.

thank you