This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: mmc2 interface not working

Part Number: AM5728


Hi

We have created custom board with reference of AM5728.

In our custom board mmc2 interface is not working.

At u-boot prompt i am not able to select mmc2 interface using command  "mmc dev 1"

Getting below error:-


=> mmc dev 1
mmc_init_stream: timedout waiting for cc!
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear

Below are the logs with other related commands for mmc interface:-

=> mmcinfo
Device: OMAP SD/MMC
Manufacturer ID: 3
OEM: 5344
Name: SS32G
Bus Speed: 48000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.7 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

=> mmc dev
switch to partitions #0, OK
mmc0 is current device


=> mmc dev 0
switch to partitions #0, OK
mmc0 is current device


=> mmc dev 1
mmc_init_stream: timedout waiting for cc!
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear
=>

Thanks & Regard

Gaurav