This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: DMTimer0 clock source

Part Number: AM3352

TI AM335x TRM Rev P spru73h.pdf

Section 8.1.6.13 Timer Clock Structure

FIgure 8-16 Watchdog Timer CLock Selection shows that Timer0 can only come from  CLK_RC_32K. The statement above the figure indicates the same. "The DMTIMER0 can only be clocked from the internal RC oscillator (CLKRC32K)."

Figure 8-17 Watchdog and Secure Timer Clock Selection shows that DMTIMER0 can come from 4 different sources.

Which is correct, Figure 8-16 or Figure 8-17?

Thanks in advance,

Paul Hetherington