Part Number: 66AK2G12
Tool/software: Linux
Hello,
I have a custom design using the 66AK2G12. We are using Linux SDK 5 with U-Boot 2018.01 and Linux 4.14.40. I have the system loading U-Boot from the SD card interface (MMCSD0). From U-Boot, I am able to load the boot files into memory and boot Linux, but the kernel boot hangs at "Waiting for root device PARTUUID=239df219-02...".
I have seen in other forum posts that this problem is often due to an issue with the chip detect. (https://e2e.ti.com/support/processors/f/791/t/553707)
Because of design constraints, we do not have a chip detect line on this design. I have added broken-cd; to the device tree node in an attempt to bypass this, but have been unsuccessful in getting the rootfs to load from the SD card.
The card was formatted with the SDK provided tool and contains a FAT partition for U-Boot and an EXT3 partition for the rootfs.
My bootargs are bootargs=console=ttyS0,115200n8 ignore_loglevel root=PARTUUID=239df219-02 rw rootfstype=ext3 rootwait
Attached is my bootlog.
Any guidance that can be provided to shine some light on why my system won't recognize the rootfs is appreciated. Please let me know if additional infomation is needed.
Thank you,
Jeff
U-Boot 2018.01-00444-g2561f9c-dirty (Jan 23 2019 - 11:38:02 -0700) CPU: 66AK2Gx-100 SR1.0 Model: Texas Instruments K2G General Purpose EVM DRAM: Clear entire DDR3 memory to enable ECC 1 GiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Net: eth0: netcp@4000000 Hit any key to stop autoboot: 0 32832 bytes read in 13 ms (2.4 MiB/s) K2_BM_15.07-53-ge1f885a SoC:k2g built:04:08:14, Jul 22 2018 ## installed monitor @ 0xc0f7000, freq [24000000], status 202338304 33620 bytes read in 14 ms (2.3 MiB/s) 0 - Name:'pmmc@2900000' type:'internal memory mapped' supports: load start Load Remote Processor 0 with data@addr=0x82000000 33620 bytes: Success! 3854848 bytes read in 187 ms (19.7 MiB/s) 34797 bytes read in 11 ms (3 MiB/s) 29850 bytes read in 15 ms (1.9 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Ramdisk to 8fff7000, end 8ffff7ed ... OK Loading Device Tree to 8ffec000, end 8fff6499 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.40-g4796173fc5 (jeff@l-serv) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #20 SMP PREEMPT Thu Jan 17 16:12:30 MST 2019 [ 0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] OF: fdt: Machine model: Texas Instruments K2G General Purpose EVM [ 0.000000] debug: ignoring loglevel setting. [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] Switching physical address space to 0x800000000 [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x000000081f800000, size 8 MiB [ 0.000000] OF: reserved mem: initialized node dsp-common-memory@81f800000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 48 MiB at 0x000000083d000000 [ 0.000000] On node 0 totalpages: 165888 [ 0.000000] free_area_init_node: node 0, pgdat c10405c0, node_mem_map d76f5000 [ 0.000000] DMA zone: 1152 pages used for memmap [ 0.000000] DMA zone: 0 pages reserved [ 0.000000] DMA zone: 100352 pages, LIFO batch:31 [ 0.000000] HighMem zone: 65536 pages, LIFO batch:15 [ 0.000000] percpu: Embedded 15 pages/cpu @d76ce000 s31308 r8192 d21940 u61440 [ 0.000000] pcpu-alloc: s31308 r8192 d21940 u61440 alloc=15*4096 [ 0.000000] pcpu-alloc: [0] 0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 164736 [ 0.000000] Kernel command line: console=ttyS0,115200n8 ignore_loglevel root=PARTUUID=239df219-02 rw rootfstype=ext3 rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 584704K/663552K available (8192K kernel code, 356K rwdata, 2472K rodata, 2048K init, 294K bss, 21504K reserved, 57344K cma-reserved, 212992K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0a00000 (10208 kB) [ 0.000000] .init : 0xc0e00000 - 0xc1000000 (2048 kB) [ 0.000000] .data : 0xc1000000 - 0xc10590c8 ( 357 kB) [ 0.000000] .bss : 0xc105b000 - 0xc10a493c ( 295 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=1. [ 0.000000] Tasks RCU enabled. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns [ 0.000004] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns [ 0.000015] Switching to timer-based delay loop, resolution 41ns [ 0.000124] keystone_timer_init: failed to get clock [ 0.000141] Failed to initialize '/soc/timer@2210000': -517 [ 0.000395] Console: colour dummy device 80x30 [ 0.000425] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000) [ 0.000440] pid_max: default: 32768 minimum: 301 [ 0.000549] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000560] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.001093] CPU: Testing write buffer coherency: ok [ 0.001309] /cpus/cpu@0 missing clock-frequency property [ 0.001323] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.040012] Setting up static identity map for 0x80200000 - 0x80200138 [ 0.060015] Hierarchical SRCU implementation. [ 0.081386] EFI services will not be available. [ 0.100084] smp: Bringing up secondary CPUs ... [ 0.100096] smp: Brought up 1 node, 1 CPU [ 0.100106] SMP: Total of 1 processors activated (48.00 BogoMIPS). [ 0.100114] CPU: All CPU(s) started in HYP mode. [ 0.100121] CPU: Virtualization extensions available. [ 0.100504] devtmpfs: initialized [ 0.105986] random: get_random_u32 called from bucket_table_alloc+0x104/0x22c with crng_init=0 [ 0.110212] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0 [ 0.110425] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.110442] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.111756] pinctrl core: initialized pinctrl subsystem [ 0.111947] DMI not present or invalid. [ 0.112194] NET: Registered protocol family 16 [ 0.120985] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.121757] cpuidle: using governor ladder [ 0.121794] cpuidle: using governor menu [ 0.122142] No ATAGs? [ 0.122184] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.122197] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.126410] davinci_gpio 2603000.gpio: could not find pctldev for node /soc/pinmux@02621000/pinmux_gpio0_pins, deferring probe [ 0.126862] davinci_gpio 260a000.gpio: could not find pctldev for node /soc/pinmux@02621000/pinmux_gpio1_pins, deferring probe [ 0.172089] i2c_davinci 2530000.i2c: could not find pctldev for node /soc/pinmux@02621000/pinmux_i2c0_pins, deferring probe [ 0.172131] i2c_davinci 2530400.i2c: could not find pctldev for node /soc/pinmux@02621000/pinmux_i2c1_pins, deferring probe [ 0.172166] i2c_davinci 2530800.i2c: could not find pctldev for node /soc/pinmux@02621000/pinmux_i2c2_pins, deferring probe [ 0.172320] media: Linux media interface: v0.10 [ 0.172361] Linux video capture interface: v2.00 [ 0.172438] pps_core: LinuxPPS API ver. 1 registered [ 0.172447] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.172467] PTP clock support registered [ 0.172484] EDAC MC: Ver: 3.0.0 [ 0.180408] dmi: Firmware registration failed. [ 0.190497] clocksource: Switched to clocksource arch_sys_counter [ 0.197818] NET: Registered protocol family 2 [ 0.198334] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.198374] TCP bind hash table entries: 4096 (order: 3, 32768 bytes) [ 0.198442] TCP: Hash tables configured (established 4096 bind 4096) [ 0.198517] UDP hash table entries: 256 (order: 1, 8192 bytes) [ 0.198540] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) [ 0.198653] NET: Registered protocol family 1 [ 0.230594] RPC: Registered named UNIX socket transport module. [ 0.230606] RPC: Registered udp transport module. [ 0.230614] RPC: Registered tcp transport module. [ 0.230621] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.230633] PCI: CLS 0 bytes, default 64 [ 0.230816] Trying to unpack rootfs image as initramfs... [ 0.233231] Freeing initrd memory: 36K [ 0.233494] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.233688] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available [ 0.234345] platform alarmtimer: set dma_pfn_offset00780000 [ 0.235010] workingset: timestamp_bits=14 max_order=18 bucket_order=4 [ 0.239223] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.250841] NFS: Registering the id_resolver key type [ 0.250866] Key type id_resolver registered [ 0.250876] Key type id_legacy registered [ 0.250914] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.252641] bounce: pool size: 64 pages [ 0.252697] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.252708] io scheduler noop registered [ 0.252717] io scheduler deadline registered [ 0.252872] io scheduler cfq registered (default) [ 0.252882] io scheduler mq-deadline registered [ 0.252891] io scheduler kyber registered [ 0.253192] keystone_irq soc:keystone_irq@026202a0: irqchip registered, nr_irqs 28 [ 0.253960] pinctrl-single 2621000.pinmux: please update dts to use #pinctrl-cells = <1> [ 0.254339] pinctrl-single 2621000.pinmux: 260 pins at pa e0850000 size 1040 [ 0.254794] gpio-syscon soc:keystone_dsp_gpio@02620240: can't read the dir register offset! [ 0.254816] gpiochip_find_base: found new base at 484 [ 0.254979] gpio gpiochip0: (soc:keystone_dsp_gpio@02620240): added GPIO chardev (254:0) [ 0.255053] gpiochip_setup_dev: registered GPIOs 484 to 511 on device: gpiochip0 (soc:keystone_dsp_gpio@02620240) [ 0.255143] gpio-syscon soc:keystone_pruss_gpio0: can't read the dir register offset! [ 0.255162] gpiochip_find_base: found new base at 456 [ 0.255295] gpio gpiochip1: (soc:keystone_pruss_gpio0): added GPIO chardev (254:1) [ 0.255368] gpiochip_setup_dev: registered GPIOs 456 to 483 on device: gpiochip1 (soc:keystone_pruss_gpio0) [ 0.255455] gpio-syscon soc:keystone_pruss_gpio1: can't read the dir register offset! [ 0.255472] gpiochip_find_base: found new base at 428 [ 0.255589] gpio gpiochip2: (soc:keystone_pruss_gpio1): added GPIO chardev (254:2) [ 0.255660] gpiochip_setup_dev: registered GPIOs 428 to 455 on device: gpiochip2 (soc:keystone_pruss_gpio1) [ 0.255744] gpio-syscon soc:keystone_pruss_gpio2: can't read the dir register offset! [ 0.255761] gpiochip_find_base: found new base at 400 [ 0.255936] gpio gpiochip3: (soc:keystone_pruss_gpio2): added GPIO chardev (254:3) [ 0.256004] gpiochip_setup_dev: registered GPIOs 400 to 427 on device: gpiochip3 (soc:keystone_pruss_gpio2) [ 0.256090] gpio-syscon soc:keystone_pruss_gpio3: can't read the dir register offset! [ 0.256106] gpiochip_find_base: found new base at 372 [ 0.256231] gpio gpiochip4: (soc:keystone_pruss_gpio3): added GPIO chardev (254:4) [ 0.256300] gpiochip_setup_dev: registered GPIOs 372 to 399 on device: gpiochip4 (soc:keystone_pruss_gpio3) [ 0.314550] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.314634] platform serial8250: set dma_pfn_offset00780000 [ 0.326464] brd: module loaded [ 0.332340] loop: module loaded [ 0.334890] platform Fixed MDIO bus.0: set dma_pfn_offset00780000 [ 0.335023] mdio_bus fixed-0: GPIO lookup for consumer reset [ 0.335034] mdio_bus fixed-0: using lookup tables for GPIO lookup [ 0.335047] mdio_bus fixed-0: lookup for GPIO reset failed [ 0.335074] libphy: Fixed MDIO Bus: probed [ 0.336796] i2c /dev entries driver [ 0.337233] IR NEC protocol handler initialized [ 0.337243] IR RC5(x/sz) protocol handler initialized [ 0.337252] IR RC6 protocol handler initialized [ 0.337259] IR JVC protocol handler initialized [ 0.337266] IR Sony protocol handler initialized [ 0.337273] IR SANYO protocol handler initialized [ 0.337279] IR Sharp protocol handler initialized [ 0.337287] IR MCE Keyboard/mouse protocol handler initialized [ 0.337294] IR XMP protocol handler initialized [ 0.338476] sdhci: Secure Digital Host Controller Interface driver [ 0.338484] sdhci: Copyright(c) Pierre Ossman [ 0.338712] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.339688] ledtrig-cpu: registered to indicate activity on CPUs [ 0.341857] NET: Registered protocol family 10 [ 0.360831] Segment Routing with IPv6 [ 0.360902] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 0.361423] NET: Registered protocol family 17 [ 0.361596] Key type dns_resolver registered [ 0.361746] Registering SWP/SWPB emulation handler [ 0.363326] GPIO line 115 (gpio0-default-lows) hogged as output/low [ 0.363350] GPIO line 50 (gpio0-default-highs) hogged as output/high [ 0.363516] gpio gpiochip5: (davinci_gpio.0): added GPIO chardev (254:5) [ 0.363593] gpiochip_setup_dev: registered GPIOs 0 to 143 on device: gpiochip5 (davinci_gpio.0) [ 0.363623] davinci_gpio 2603000.gpio: Error -517 getting gpio clock [ 0.364304] GPIO line 39 (gpio1-defaults) hogged as output/high [ 0.364445] gpio gpiochip5: (davinci_gpio.0): added GPIO chardev (254:5) [ 0.364523] gpiochip_setup_dev: registered GPIOs 0 to 67 on device: gpiochip5 (davinci_gpio.0) [ 0.364552] davinci_gpio 260a000.gpio: Error -517 getting gpio clock [ 0.370432] ti-sci 2921c00.pmmc: ABI: 2.4 (firmware rev 0x0011 '0.1.1-50-g129ef (Eagle)') [ 0.386583] random: fast init done [ 0.405482] ti-sci-clk 2921c00.pmmc:clocks: get-parent failed for dev=76, clk=11, ret=-19 [ 0.405599] ti-sci-clk 2921c00.pmmc:clocks: get-parent failed for dev=76, clk=11, ret=-19 [ 0.405847] ti-sci-clk 2921c00.pmmc:clocks: get-parent failed for dev=76, clk=11, ret=-19 [ 0.411767] keystone timer clock @166666666 Hz [ 0.412102] GPIO line 115 (gpio0-default-lows) hogged as output/low [ 0.412124] GPIO line 50 (gpio0-default-highs) hogged as output/high [ 0.412289] gpio gpiochip5: (davinci_gpio.0): added GPIO chardev (254:5) [ 0.412367] gpiochip_setup_dev: registered GPIOs 0 to 143 on device: gpiochip5 (davinci_gpio.0) [ 0.415823] GPIO line 183 (gpio1-defaults) hogged as output/high [ 0.415980] gpio gpiochip6: (davinci_gpio.1): added GPIO chardev (254:6) [ 0.416059] gpiochip_setup_dev: registered GPIOs 144 to 211 on device: gpiochip6 (davinci_gpio.1) [ 0.422284] edma 2700000.edma: TI EDMA DMA engine driver [ 0.422779] edma 2728000.edma: memcpy is disabled [ 0.426107] edma 2728000.edma: TI EDMA DMA engine driver [ 0.429020] keystone-navigator-qmss soc:qmss@4020000: qmgr start queue 0, number of queues 128 [ 0.429138] keystone-navigator-qmss soc:qmss@4020000: added qmgr start queue 0, num of queues 128, reg_peek e0e61000, reg_status (null), reg_config e0e63000, reg_region e0e65000, reg_push e0e67000, reg_pop e0e67000 [ 0.430091] keystone-navigator-dma soc:knav_dmas@0: DMA dma_gbe registered 53 logical channels, flows 32, tx chans: 21, rx chans: 32 [ 0.431095] console [ttyS0] disabled [ 0.431132] 2530c00.serial: ttyS0 at MMIO 0x2530c00 (irq = 23, base_baud = 12000000) is a TI DA8xx/66AK2x [ 1.721266] console [ttyS0] enabled [ 1.725892] 2531000.serial: ttyS1 at MMIO 0x2531000 (irq = 24, base_baud = 12000000) is a TI DA8xx/66AK2x [ 1.736628] 2531400.serial: ttyS2 at MMIO 0x2531400 (irq = 25, base_baud = 12000000) is a TI DA8xx/66AK2x [ 1.747061] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805400[0]' [ 1.756243] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805400[1]' [ 1.765399] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805400[2]' [ 1.774532] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805400[3]' [ 1.783664] spi_davinci 21805400.spi: DMA is not supported (-19) [ 1.790198] spidev spi0.0: buggy DT: spidev listed directly in DT [ 2.275390] spidev spi0.1: buggy DT: spidev listed directly in DT [ 2.761511] spi_davinci 21805400.spi: Controller at 0xe0e79400 [ 2.768137] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805800[0]' [ 2.777318] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805800[1]' [ 2.786453] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805800[2]' [ 2.795618] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805800[3]' [ 2.804752] spi_davinci 21805800.spi: DMA is not supported (-19) [ 2.811306] spidev spi1.0: buggy DT: spidev listed directly in DT [ 3.297664] spidev spi1.1: buggy DT: spidev listed directly in DT [ 3.783778] spi_davinci 21805800.spi: Controller at 0xe0e7b800 [ 3.790253] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805c00[0]' [ 3.799398] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805c00[1]' [ 3.808531] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805c00[2]' [ 3.817660] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21805c00[3]' [ 3.826790] spi_davinci 21805c00.spi: DMA is not supported (-19) [ 3.833327] spidev spi2.0: buggy DT: spidev listed directly in DT [ 4.319665] spidev spi2.1: buggy DT: spidev listed directly in DT [ 4.805980] spidev spi2.2: buggy DT: spidev listed directly in DT [ 5.292087] spi_davinci 21805c00.spi: Controller at 0xe0e7dc00 [ 5.298558] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21806000[0]' [ 5.307705] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21806000[1]' [ 5.316837] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21806000[2]' [ 5.325968] of_get_named_gpiod_flags: can't parse 'cs-gpios' property of node '/soc/spi@21806000[3]' [ 5.335101] spi_davinci 21806000.spi: DMA is not supported (-19) [ 5.341713] m25p80 spi3.0: found s25fl064l, expected s25sl032p [ 5.347938] m25p80 spi3.0: s25fl064l (8192 Kbytes) [ 5.352760] 1 ofpart partitions found on MTD device spi3.0 [ 5.358232] Creating 1 MTD partitions on "spi3.0": [ 5.363034] 0x000000000000-0x000000100000 : "xmos-img" [ 5.369152] spidev spi3.1: buggy DT: spidev listed directly in DT [ 5.855319] spi_davinci 21806000.spi: Controller at 0xe0e7f000 [ 5.861648] mdio_bus 4200f00.mdio: GPIO lookup for consumer reset [ 5.867731] mdio_bus 4200f00.mdio: using device tree for GPIO lookup [ 5.874101] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/soc/mdio@4200f00[0]' [ 5.883492] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/soc/mdio@4200f00[0]' [ 5.892794] mdio_bus 4200f00.mdio: using lookup tables for GPIO lookup [ 5.899310] mdio_bus 4200f00.mdio: lookup for GPIO reset failed [ 5.960520] davinci_mdio 4200f00.mdio: davinci mdio revision 1.7, bus freq 2500000 [ 5.968074] libphy: 4200f00.mdio: probed [ 5.972846] davinci_mdio 4200f00.mdio: phy[0]: device 4200f00.mdio:00, driver TI DP83867 [ 5.981491] netcp-1.0 2620110.netcp: ALE enabled [ 5.986229] netcp-1.0 2620110.netcp: initialized cpsw ale version 1.4 [ 5.992720] netcp-1.0 2620110.netcp: ALE Table size 64 [ 5.997914] netcp-1.0 2620110.netcp: cpts: overflow check period 500 (jiffies) [ 6.005187] netcp-1.0 2620110.netcp: CPTS: ref_clk_freq:250000000 calc_mult:2147483648 calc_shift:29 error:0 nsec/sec [ 6.016460] netcp-1.0 2620110.netcp: module(netcp-xgbe) not used for device [ 6.023855] Probing sdhci! [ 6.026657] sdhci-omap 23000000.mmc: GPIO lookup for consumer wp [ 6.032681] sdhci-omap 23000000.mmc: using device tree for GPIO lookup [ 6.039202] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/soc/mmc@23000000[0]' [ 6.048334] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/soc/mmc@23000000[0]' [ 6.057375] sdhci-omap 23000000.mmc: using lookup tables for GPIO lookup [ 6.064077] sdhci-omap 23000000.mmc: lookup for GPIO wp failed [ 6.069992] sdhci: no write protect flag set [ 6.074430] mmc0: Hardware doesn't report any support voltages. [ 6.080989] hctosys: unable to open rtc device (rtc0) [ 6.109924] Waiting for root device PARTUUID=239df219-02...