This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 Will be waked earlier than TPS6930 on evm2 board?

Other Parts Discussed in Thread: TPS65930, OMAP3530

hi,all:

            I tested the sleep/wakeup feature on evm2 board ,I find that  the "sys_off_mode" will be changed to high earlier than vdd1/vdd2  when wakeup,  and then,can I confirm that OMAP3530 Will be waked earlier  than TPS6930 ? if so, it will be error when OMAP3530 run but part Power supply which controlled by tps65930 is off .

  • There are several voltage domain in OMAP3530. Figure 1-79 in  OMAP3530 TRM (chapter 1.10 PRCM Voltage Management Functional Description) gives a good overview of the device voltage domains.

    VDD1 provides power to MPU and IVA power domain, and VDD2 provides power to CORE/PER etc

    While VDD1 and VDD2 are in OFF mode, the wakeup domain is not powered off. Its power comes from VDD3 voltage domain.

    Thanks,

    Tao