Other Parts Discussed in Thread: SYSBIOS,
Tool/software: TI-RTOS
Currently, we are porting from "AM574x" to "AM335x",
There are some questions about the environment construction of "AM335x".
Question 1
C:\ti\bios_6_73_00_12\packages\ti\sysbios\family\shared\vayu\IntXbar.xs
C:\ti\bios_6_73_00_12\packages\ti\sysbios\family\shared\vayu\TimerSupport.xs
When I execute "xdc.useModule", "Target A8F is not supported!" Error occurs. Are "IntXbar" and "TimerSupport" features not supported on AM335x?
If not, are there plans for future support?
Question 2
Because "biosTimer.h" does not exist in "pdk_am335x_1_0_12", a "No such file or directory" error occurs at build time. Is the "biosTimer" feature not supported on AM335x?
If not, are there plans for future support?
The environment is as follows.
HW:SK_AM3358
soc:am335x
CCS v8.1.0
GCC GNU v6.3.1(Linaro)
bios_6_73_00_12
ndk_2_26_00_08
pdk_am335x_1_0_12
xdctools_3_50_03_33_core
I hope you have a good answer.
best regards.