This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Binaries of Gstreamer for EVM357



Hi

I need to test Gstreamer in my EVM357 in a hurry.

I haven't the packages for compiling it in my Linux host yet. I am using Ubuntu.

According with my past experience, I will face a lot of variables before I can compile smoothly the binaries of Gstreamer for EVM357.

So, I want to question if already exists binaries of Gstreamer for EVM357 available somewhere, ready to run.

I know that sooner or later I will need to install the packages to proceed with the development, but, what I want to know right now is that if Gstreamer really is a solution for my problem. I need to build a H.264 audio/video streamer server ( like an IP camera using external camera ). And, more important, if DM357 really works fine with Gstreamer. I explain why I am so carefull about: I went from a failed project of a video streamer using iMX31LC, that consumed 2 years of hard work, to find stucked with a kernel linux with lot of lacks that failed to run Gstreamer reliably. As a matter of fact, Gstreamer NEVER worked in the iMX31LC.

I will appreciate any help about.

Thanks